how can i use MPX5700DP?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how can i use MPX5700DP?

2,090 次查看
kgn2891
Contributor I

mpx5700dp output can use 5Voltage in datasheet but

i diagnose pin1(OUT) to only max 1Voltage  when i use pin3(5V),pin2(GND) without pin4,5,6 

attact the circuit i used.

is it wrong method?

0 项奖励
回复
1 回复

2,037 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Kim,

Your connection is correct. 

V1, V2 and Vex pins are used for factory trimming and we recommend to leave these pins unconnected/floating.

Only pin #1 (Vout), pin #2 (Ground) and pin #3 (Vs) are required as shown in Figure 1 of the data sheet.

The MPX5700DP measures the difference between pressures applied simultaneously to opposite sides of the diaphragm:

pastedImage_10.png

The transfer function and characteristic:

pastedImage_4.png

Best regards,

Tomas

0 项奖励
回复