how can i use MPX5700DP?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how can i use MPX5700DP?

2,084件の閲覧回数
kgn2891
Contributor I

mpx5700dp output can use 5Voltage in datasheet but

i diagnose pin1(OUT) to only max 1Voltage  when i use pin3(5V),pin2(GND) without pin4,5,6 

attact the circuit i used.

is it wrong method?

0 件の賞賛
返信
1 返信

2,031件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Kim,

Your connection is correct. 

V1, V2 and Vex pins are used for factory trimming and we recommend to leave these pins unconnected/floating.

Only pin #1 (Vout), pin #2 (Ground) and pin #3 (Vs) are required as shown in Figure 1 of the data sheet.

The MPX5700DP measures the difference between pressures applied simultaneously to opposite sides of the diaphragm:

pastedImage_10.png

The transfer function and characteristic:

pastedImage_4.png

Best regards,

Tomas

0 件の賞賛
返信