how can i use MPX5700DP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how can i use MPX5700DP?

2,080 Views
kgn2891
Contributor I

mpx5700dp output can use 5Voltage in datasheet but

i diagnose pin1(OUT) to only max 1Voltage  when i use pin3(5V),pin2(GND) without pin4,5,6 

attact the circuit i used.

is it wrong method?

0 Kudos
Reply
1 Reply

2,027 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Kim,

Your connection is correct. 

V1, V2 and Vex pins are used for factory trimming and we recommend to leave these pins unconnected/floating.

Only pin #1 (Vout), pin #2 (Ground) and pin #3 (Vs) are required as shown in Figure 1 of the data sheet.

The MPX5700DP measures the difference between pressures applied simultaneously to opposite sides of the diaphragm:

pastedImage_10.png

The transfer function and characteristic:

pastedImage_4.png

Best regards,

Tomas

0 Kudos
Reply