Which set of pin names to use for MPXV5010DP?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which set of pin names to use for MPXV5010DP?

ソリューションへジャンプ
2,149件の閲覧回数
kam-fei_leong
Contributor I

Hi,

For part number MPXV5010DP, please advise on which set of pin names / pin functions to use.

https://www.nxp.com/docs/en/data-sheet/MPX5010.pdf

Page 14 of the datasheet (per link above) shows 2 sets of pin names / pin functions, namely "Style 1" and "Style 2".

Regards,

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,047件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Fei,

The MPXV5010DP is an integrated pressure sensor so you have to use Style 2. Please note that there are also compensated pressure sensors in the same package. These devices have differential output (+Vout, -Vout) and then Style 1 is used.

 

So, the pin description is as follows:

 

1 – N/C

2 – Vs

3 – GND

4 – Vout

5 – N/C

6 – N/C

7 – N/C

8 – N/C

 

You can find it also in Figure 1 of the datasheet:

pastedImage_3.png

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,046件の閲覧回数
kam-fei_leong
Contributor I

Huge thanks to TomasVaverka‌.

0 件の賞賛
返信
2,048件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Fei,

The MPXV5010DP is an integrated pressure sensor so you have to use Style 2. Please note that there are also compensated pressure sensors in the same package. These devices have differential output (+Vout, -Vout) and then Style 1 is used.

 

So, the pin description is as follows:

 

1 – N/C

2 – Vs

3 – GND

4 – Vout

5 – N/C

6 – N/C

7 – N/C

8 – N/C

 

You can find it also in Figure 1 of the datasheet:

pastedImage_3.png

Best regards,

Tomas

0 件の賞賛
返信