Which set of pin names to use for MPXV5010DP?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which set of pin names to use for MPXV5010DP?

Jump to solution
1,135 Views
kam-fei_leong
Contributor I

Hi,

For part number MPXV5010DP, please advise on which set of pin names / pin functions to use.

https://www.nxp.com/docs/en/data-sheet/MPX5010.pdf

Page 14 of the datasheet (per link above) shows 2 sets of pin names / pin functions, namely "Style 1" and "Style 2".

Regards,

Labels (1)
Tags (2)
0 Kudos
1 Solution
1,032 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Fei,

The MPXV5010DP is an integrated pressure sensor so you have to use Style 2. Please note that there are also compensated pressure sensors in the same package. These devices have differential output (+Vout, -Vout) and then Style 1 is used.

 

So, the pin description is as follows:

 

1 – N/C

2 – Vs

3 – GND

4 – Vout

5 – N/C

6 – N/C

7 – N/C

8 – N/C

 

You can find it also in Figure 1 of the datasheet:

pastedImage_3.png

Best regards,

Tomas

View solution in original post

0 Kudos
2 Replies
1,032 Views
kam-fei_leong
Contributor I

Huge thanks to TomasVaverka‌.

0 Kudos
1,033 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Fei,

The MPXV5010DP is an integrated pressure sensor so you have to use Style 2. Please note that there are also compensated pressure sensors in the same package. These devices have differential output (+Vout, -Vout) and then Style 1 is used.

 

So, the pin description is as follows:

 

1 – N/C

2 – Vs

3 – GND

4 – Vout

5 – N/C

6 – N/C

7 – N/C

8 – N/C

 

You can find it also in Figure 1 of the datasheet:

pastedImage_3.png

Best regards,

Tomas

0 Kudos