Which set of pin names to use for MPXV5010DP?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which set of pin names to use for MPXV5010DP?

跳至解决方案
2,088 次查看
kam-fei_leong
Contributor I

Hi,

For part number MPXV5010DP, please advise on which set of pin names / pin functions to use.

https://www.nxp.com/docs/en/data-sheet/MPX5010.pdf

Page 14 of the datasheet (per link above) shows 2 sets of pin names / pin functions, namely "Style 1" and "Style 2".

Regards,

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,985 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Fei,

The MPXV5010DP is an integrated pressure sensor so you have to use Style 2. Please note that there are also compensated pressure sensors in the same package. These devices have differential output (+Vout, -Vout) and then Style 1 is used.

 

So, the pin description is as follows:

 

1 – N/C

2 – Vs

3 – GND

4 – Vout

5 – N/C

6 – N/C

7 – N/C

8 – N/C

 

You can find it also in Figure 1 of the datasheet:

pastedImage_3.png

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,985 次查看
kam-fei_leong
Contributor I

Huge thanks to TomasVaverka‌.

0 项奖励
回复
1,986 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Fei,

The MPXV5010DP is an integrated pressure sensor so you have to use Style 2. Please note that there are also compensated pressure sensors in the same package. These devices have differential output (+Vout, -Vout) and then Style 1 is used.

 

So, the pin description is as follows:

 

1 – N/C

2 – Vs

3 – GND

4 – Vout

5 – N/C

6 – N/C

7 – N/C

8 – N/C

 

You can find it also in Figure 1 of the datasheet:

pastedImage_3.png

Best regards,

Tomas

0 项奖励
回复