Vibrations measure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vibrations measure

1,245 Views
maurogatti
Contributor I

Hi, I have to design a device to measure the vibration on the splindle of mechanical machine. I already used the MMA8451 accelerometer to measurement of inclination; for us, could I use it also to measure the vibration? Best regards.

Labels (1)
0 Kudos
Reply
2 Replies

1,062 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mauro,

The MMA8451Q might be a good choice, but we need more information such as the frequency of vibration, since vibration sensing is limited by an internal filtering in an accelerometer.

Best regards,

Tomas

0 Kudos
Reply

1,062 Views
maurogatti
Contributor I

The  spindle can run at 30000 rpm so the frequency is 500 Hz

0 Kudos
Reply