Hi, is there a way to save the i2c free programmable slave address of MMA995xL sensor module ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hi, is there a way to save the i2c free programmable slave address of MMA995xL sensor module ?

1,356 次查看
nxp_user
Contributor I

Hi, is there a way to save the i2c free programmable slave address of MMA995xL sensor module ?

标签 (1)
0 项奖励
回复
3 回复数

1,156 次查看
nxp_user
Contributor I

MMA9550L

Thanks

0 项奖励
回复

1,156 次查看
JackITB
NXP Employee
NXP Employee

Ok thanks,

One possibility is to do this "programmatically": i.e. add a custom application that changes the Slave Port Address during MMA9550L initialization (see SP_ADDR register in MMA955xL Hardware Reference manual p.108). You can find information about developing custom user application in AN4129.

Regards,   Jacques.

0 项奖励
回复

1,156 次查看
JackITB
NXP Employee
NXP Employee

Hi Enrico,

Yes, this should be doable. Nevertheless we need more information from you, more specifically which version are you considering (between MMA9550, MMA9551, MMA9553, MMA9555, MMA9559...), as their Firmware differ and may be a limiting factor.

Regards,   Jacques.

0 项奖励
回复