Vibrations measure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Vibrations measure

1,267 次查看
maurogatti
Contributor I

Hi, I have to design a device to measure the vibration on the splindle of mechanical machine. I already used the MMA8451 accelerometer to measurement of inclination; for us, could I use it also to measure the vibration? Best regards.

标签 (1)
0 项奖励
回复
2 回复数

1,084 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mauro,

The MMA8451Q might be a good choice, but we need more information such as the frequency of vibration, since vibration sensing is limited by an internal filtering in an accelerometer.

Best regards,

Tomas

0 项奖励
回复

1,084 次查看
maurogatti
Contributor I

The  spindle can run at 30000 rpm so the frequency is 500 Hz

0 项奖励
回复