Sensor Toolbox

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Sensor Toolbox

跳至解决方案
4,310 次查看
sbrack
Contributor I

Hello All,

I have only played around with the functions on the sensor toolbox a little, but is there a way to record the magnetic readings with the program?

Thanks

Sam

标签 (1)
0 项奖励
回复
1 解答
3,999 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sam,

If you are using the RD4247MAG3110 kit, please download and install the E-Compass Sensor Toolbox v6.1.0.1. Then you can start data recording by pressing the Start button in the Data Log frame of the GUI. For more information please refer to Chapter 9 of the E-Compass Sensor Toolbox User Guide.

It is also possible to collect raw data from generic terminal program such as RealTerm using the commands described in the attached document.

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

在原帖中查看解决方案

3 回复数
3,999 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sam,

Could you please specify which evaluation board and Sensor Toolbox version you are using?

Regards,

Tomas

0 项奖励
回复
3,999 次查看
sbrack
Contributor I

I am using a LFSTBUSB interface board with the Sensor Toolbox v4.2.1.20.​ I purchased the RD4247MAG3110 magnetic sensor kit, and I am looking to record some of the magnetic readings using the sensor toolbox. If that is possible.

Thanks

Sam

0 项奖励
回复
4,000 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sam,

If you are using the RD4247MAG3110 kit, please download and install the E-Compass Sensor Toolbox v6.1.0.1. Then you can start data recording by pressing the Start button in the Data Log frame of the GUI. For more information please refer to Chapter 9 of the E-Compass Sensor Toolbox User Guide.

It is also possible to collect raw data from generic terminal program such as RealTerm using the commands described in the attached document.

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.