Hi Cesar,
1. Terminal Finish:
Plating on the leads is NiPdAu.
2. ESD Level:
NXP Pressure sensors are Class 1 ESD, so it has a range up to 2000 Volts (ESD).
Electrostatic Discharge will applied according Human Body Model (HBM); Test @ 500/1000/1500/2000 Volts.
3. MSL Level:
MSL = n/a because it is an open cavity device.
Have a great day,
Jose
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------