Sensor Toolbox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,027件の閲覧回数
sbrack
Contributor I

Hello All,

I have only played around with the functions on the sensor toolbox a little, but is there a way to record the magnetic readings with the program?

Thanks

Sam

ラベル(1)
0 件の賞賛
返信
1 解決策
3,716件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sam,

If you are using the RD4247MAG3110 kit, please download and install the E-Compass Sensor Toolbox v6.1.0.1. Then you can start data recording by pressing the Start button in the Data Log frame of the GUI. For more information please refer to Chapter 9 of the E-Compass Sensor Toolbox User Guide.

It is also possible to collect raw data from generic terminal program such as RealTerm using the commands described in the attached document.

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

元の投稿で解決策を見る

3 返答(返信)
3,716件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sam,

Could you please specify which evaluation board and Sensor Toolbox version you are using?

Regards,

Tomas

0 件の賞賛
返信
3,716件の閲覧回数
sbrack
Contributor I

I am using a LFSTBUSB interface board with the Sensor Toolbox v4.2.1.20.​ I purchased the RD4247MAG3110 magnetic sensor kit, and I am looking to record some of the magnetic readings using the sensor toolbox. If that is possible.

Thanks

Sam

0 件の賞賛
返信
3,717件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sam,

If you are using the RD4247MAG3110 kit, please download and install the E-Compass Sensor Toolbox v6.1.0.1. Then you can start data recording by pressing the Start button in the Data Log frame of the GUI. For more information please refer to Chapter 9 of the E-Compass Sensor Toolbox User Guide.

It is also possible to collect raw data from generic terminal program such as RealTerm using the commands described in the attached document.

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.