Need help in selecting a Sensor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need help in selecting a Sensor

743 次查看
radheshpulimutt
Contributor I

Hello, For my Mater thesis I am developing an Interactive Globe, for which I require a sensor which can sense TOUCH. The user will be touching a continent and this should result in stating the respective name of the continent. The problem I am facing is that the user won't be touching the sensor directly. Can anybody suggest a sensor for this application???

0 项奖励
回复
1 回复

639 次查看
darioarias
NXP Employee
NXP Employee

Hi Radhesh,

The portfolio of low-power touch sensors use the human body as one of the capacitive plates of an electrical circuit.  Capacitive sensors can also switch without contact due to proximity sensing or used with external plates connected to the device. I think this type of sensor are suitable for your application where the external plate is shaped as a continent. The sensors we have are, PCF8883 and PCF8885.

Hope you found them useful

Darío

0 项奖励
回复