Need help in selecting a Sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need help in selecting a Sensor

746件の閲覧回数
radheshpulimutt
Contributor I

Hello, For my Mater thesis I am developing an Interactive Globe, for which I require a sensor which can sense TOUCH. The user will be touching a continent and this should result in stating the respective name of the continent. The problem I am facing is that the user won't be touching the sensor directly. Can anybody suggest a sensor for this application???

0 件の賞賛
返信
1 返信

642件の閲覧回数
darioarias
NXP Employee
NXP Employee

Hi Radhesh,

The portfolio of low-power touch sensors use the human body as one of the capacitive plates of an electrical circuit.  Capacitive sensors can also switch without contact due to proximity sensing or used with external plates connected to the device. I think this type of sensor are suitable for your application where the external plate is shaped as a continent. The sensors we have are, PCF8883 and PCF8885.

Hope you found them useful

Darío

0 件の賞賛
返信