MPXH6400AC6T1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,694件の閲覧回数
cwtengr
Contributor I

There are 4 pins that state "Do not connect to external circuitry or ground." Is it recommended to connect these DNC pins together to provide better structural strength for the sensor? Will this affect any signals? Removing tubing can sometimes cause the sensor to be ripped from the PCB.

0 件の賞賛
1 解決策
2,685件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

These pins must be leave unconnected since these pins are used for factory calibration, you must not connect to external circuitry or ground, otherwise you will probably change the calibrations values causing a malfunction of the device, or even worst, the device could be permanently damaged.

So, as I mentioned before, I do recommend leave these pins unconnected.

I hope this information will be useful for you. I am glad to help.

Best regards,

David

元の投稿で解決策を見る

0 件の賞賛
1 返信
2,686件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello,

These pins must be leave unconnected since these pins are used for factory calibration, you must not connect to external circuitry or ground, otherwise you will probably change the calibrations values causing a malfunction of the device, or even worst, the device could be permanently damaged.

So, as I mentioned before, I do recommend leave these pins unconnected.

I hope this information will be useful for you. I am glad to help.

Best regards,

David

0 件の賞賛