MPX5700 maximum temperature for mounting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPX5700 maximum temperature for mounting

ソリューションへジャンプ
1,733件の閲覧回数
joaoramos
Contributor I

ABOUT MPX5700

What is the maximum temperature that the sensor withstands in the soldering oven?

I want to oven a PCB for a 60 minute cycle at 240°C.
Will this damage the sensor?

The data sheet informs that it supports working up to 125°C, I just want to solder it at a high temperature, After the use will be moderate.

0 件の賞賛
返信
1 解決策
1,718件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello João,

As you can see on this website or in the AN3150, the MPX5700 should not be exposed to temperatures higher than 220°C for more than 30s.

Best regards,

Tomas

元の投稿で解決策を見る

2 返答(返信)
1,709件の閲覧回数
joaoramos
Contributor I

Exactly the document I was looking for!!
Thanks Tomas!

0 件の賞賛
返信
1,719件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello João,

As you can see on this website or in the AN3150, the MPX5700 should not be exposed to temperatures higher than 220°C for more than 30s.

Best regards,

Tomas