MPX5700 maximum temperature for mounting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPX5700 maximum temperature for mounting

跳至解决方案
1,580 次查看
joaoramos
Contributor I

ABOUT MPX5700

What is the maximum temperature that the sensor withstands in the soldering oven?

I want to oven a PCB for a 60 minute cycle at 240°C.
Will this damage the sensor?

The data sheet informs that it supports working up to 125°C, I just want to solder it at a high temperature, After the use will be moderate.

0 项奖励
回复
1 解答
1,565 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello João,

As you can see on this website or in the AN3150, the MPX5700 should not be exposed to temperatures higher than 220°C for more than 30s.

Best regards,

Tomas

在原帖中查看解决方案

2 回复数
1,556 次查看
joaoramos
Contributor I

Exactly the document I was looking for!!
Thanks Tomas!

0 项奖励
回复
1,566 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello João,

As you can see on this website or in the AN3150, the MPX5700 should not be exposed to temperatures higher than 220°C for more than 30s.

Best regards,

Tomas