MPX5700 maximum temperature for mounting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPX5700 maximum temperature for mounting

Jump to solution
1,732 Views
joaoramos
Contributor I

ABOUT MPX5700

What is the maximum temperature that the sensor withstands in the soldering oven?

I want to oven a PCB for a 60 minute cycle at 240°C.
Will this damage the sensor?

The data sheet informs that it supports working up to 125°C, I just want to solder it at a high temperature, After the use will be moderate.

0 Kudos
Reply
1 Solution
1,717 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello João,

As you can see on this website or in the AN3150, the MPX5700 should not be exposed to temperatures higher than 220°C for more than 30s.

Best regards,

Tomas

View solution in original post

2 Replies
1,708 Views
joaoramos
Contributor I

Exactly the document I was looking for!!
Thanks Tomas!

0 Kudos
Reply
1,718 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello João,

As you can see on this website or in the AN3150, the MPX5700 should not be exposed to temperatures higher than 220°C for more than 30s.

Best regards,

Tomas