MPX5100 - Vacuum Measurement

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPX5100 - Vacuum Measurement

跳至解决方案
1,669 次查看
WRGandolphini
Contributor I

Hi, I would like some information about the MPX5100DP sensor.

I need to perform a measurement on an electromedical equipment and this makes a vacuum inside suction cups that are attached to the patient.

The measurement range would be from 0kpa to -100kpa.

Could you use this sensor for this purpose?

 

Thanks

0 项奖励
回复
1 解答
1,654 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Roberto,

I believe you can use the MPX5100DP for this purpose. As long as the pressure difference between P1 and P2 is less than 100kPa and P1>P2, there will be no issue.

You can also consider using the MPXV6115VC6U gauge vacuum sensor.

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,655 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Roberto,

I believe you can use the MPX5100DP for this purpose. As long as the pressure difference between P1 and P2 is less than 100kPa and P1>P2, there will be no issue.

You can also consider using the MPXV6115VC6U gauge vacuum sensor.

Best regards,

Tomas

0 项奖励
回复