MPX5100 - Vacuum Measurement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPX5100 - Vacuum Measurement

ソリューションへジャンプ
1,668件の閲覧回数
WRGandolphini
Contributor I

Hi, I would like some information about the MPX5100DP sensor.

I need to perform a measurement on an electromedical equipment and this makes a vacuum inside suction cups that are attached to the patient.

The measurement range would be from 0kpa to -100kpa.

Could you use this sensor for this purpose?

 

Thanks

0 件の賞賛
返信
1 解決策
1,653件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Roberto,

I believe you can use the MPX5100DP for this purpose. As long as the pressure difference between P1 and P2 is less than 100kPa and P1>P2, there will be no issue.

You can also consider using the MPXV6115VC6U gauge vacuum sensor.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,654件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Roberto,

I believe you can use the MPX5100DP for this purpose. As long as the pressure difference between P1 and P2 is less than 100kPa and P1>P2, there will be no issue.

You can also consider using the MPXV6115VC6U gauge vacuum sensor.

Best regards,

Tomas

0 件の賞賛
返信