MM9Z1 system calibration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MM9Z1 system calibration

Jump to solution
2,658 Views
Shaojun
Contributor I

Dear support/community,

as mentioned in the datasheet(MM9Z1_638D1), a system calibration should be performed on the system level to remove effects/errors introduced through device configuration, soldering, and external components. The calibration should be performed at ~25°C.

My question is, does the temperature 25°C correspond to room temperature or Tsense chip temperature(ITS).

Thanks!

best regards,

Shaojun

0 Kudos
Reply
1 Solution
2,652 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Shaojun, 

there is an application note AN12301 describing calibration processes of the MM9Z1 temperature sensor. The calibration should be performed at room temperature ~25°C. If the chip is unused for few hours the room temperature and ITS will be the same.

With Best Regards,

Jozef

View solution in original post

0 Kudos
Reply
1 Reply
2,653 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Shaojun, 

there is an application note AN12301 describing calibration processes of the MM9Z1 temperature sensor. The calibration should be performed at room temperature ~25°C. If the chip is unused for few hours the room temperature and ITS will be the same.

With Best Regards,

Jozef

0 Kudos
Reply