MM9Z1 system calibration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MM9Z1 system calibration

ソリューションへジャンプ
2,055件の閲覧回数
Shaojun
Contributor I

Dear support/community,

as mentioned in the datasheet(MM9Z1_638D1), a system calibration should be performed on the system level to remove effects/errors introduced through device configuration, soldering, and external components. The calibration should be performed at ~25°C.

My question is, does the temperature 25°C correspond to room temperature or Tsense chip temperature(ITS).

Thanks!

best regards,

Shaojun

0 件の賞賛
返信
1 解決策
2,049件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Shaojun, 

there is an application note AN12301 describing calibration processes of the MM9Z1 temperature sensor. The calibration should be performed at room temperature ~25°C. If the chip is unused for few hours the room temperature and ITS will be the same.

With Best Regards,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,050件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Shaojun, 

there is an application note AN12301 describing calibration processes of the MM9Z1 temperature sensor. The calibration should be performed at room temperature ~25°C. If the chip is unused for few hours the room temperature and ITS will be the same.

With Best Regards,

Jozef

0 件の賞賛
返信