MC33771C idle state

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC33771C idle state

跳至解决方案
835 次查看
alessandro_piazza
Contributor II

Hi, after power up (no CSB activity, I saw VCOM fixed on it) MC33771C consume 6mA. shouldn't it go to idle state?

Thanks!

 

0 项奖励
回复
1 解答
819 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Alessandro,

please refer to the Figure 8. in the MC33771C full datasheet. The MC33771C can switch to Idle mode only from the INIT mode if the communication is not active. If the MC33771C is not initialized within 60s, then it switches to Idle mode. Please refer to the sections 9.3.2 and 9.3.3. From Normal mode you can send it to Sleep mode by software command. Please refer to section 9.3.4.

With Best Regards,

Jozef

在原帖中查看解决方案

1 回复
820 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Alessandro,

please refer to the Figure 8. in the MC33771C full datasheet. The MC33771C can switch to Idle mode only from the INIT mode if the communication is not active. If the MC33771C is not initialized within 60s, then it switches to Idle mode. Please refer to the sections 9.3.2 and 9.3.3. From Normal mode you can send it to Sleep mode by software command. Please refer to section 9.3.4.

With Best Regards,

Jozef