Aging of MMA7361L

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Aging of MMA7361L

1,313 次查看
uchidaJ
Contributor II

I would like to obtain the tilt angle using only the Z axis of MMA7361L. After the offset is calibrated at the assembly factory, if the end user uses it for 5 years without recalibrating it, what is the maximum change in tilt angle error?

4 回复数

1,271 次查看
onyourlight
Contributor III

MMA7361L  is eol

0 项奖励
回复

1,253 次查看
uchidaJ
Contributor II

Thank you for letting me know.
I'm sorry if my initial explanation was insufficient.
I posted on the forum with the intention of using parts I already own.

0 项奖励
回复

1,302 次查看
diazmarin09
NXP TechSupport
NXP TechSupport

Hello uchidaJ,

I hope all is great with you. Thank you for using the NXP communities.

It is difficult to know. There are a number of proponents when it comes to offset errors such as trim errors, mechanical stresses due to package and mounting, shifts due to temperature, and of course, aging.

Therefore, I do recommend to perform the calibration procedure periodically.

 

Please note that the MMA7361L is an obsolete device. Please let me know if you need further information for a replacement device.

I hope this information helps.

Regards,

David

0 项奖励
回复

1,286 次查看
uchidaJ
Contributor II

Thanks, David.
I understand now that you need to perform the calibration procedure periodically.
Have a nice day.