MC33771C idle state

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33771C idle state

Jump to solution
834 Views
alessandro_piazza
Contributor II

Hi, after power up (no CSB activity, I saw VCOM fixed on it) MC33771C consume 6mA. shouldn't it go to idle state?

Thanks!

 

0 Kudos
Reply
1 Solution
818 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Alessandro,

please refer to the Figure 8. in the MC33771C full datasheet. The MC33771C can switch to Idle mode only from the INIT mode if the communication is not active. If the MC33771C is not initialized within 60s, then it switches to Idle mode. Please refer to the sections 9.3.2 and 9.3.3. From Normal mode you can send it to Sleep mode by software command. Please refer to section 9.3.4.

With Best Regards,

Jozef

View solution in original post

1 Reply
819 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Alessandro,

please refer to the Figure 8. in the MC33771C full datasheet. The MC33771C can switch to Idle mode only from the INIT mode if the communication is not active. If the MC33771C is not initialized within 60s, then it switches to Idle mode. Please refer to the sections 9.3.2 and 9.3.3. From Normal mode you can send it to Sleep mode by software command. Please refer to section 9.3.4.

With Best Regards,

Jozef