MAG 3110 ctrl_reg2 reading issue.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MAG 3110 ctrl_reg2 reading issue.

2,062 次查看
nicolasdecroze
Contributor I

Hello,

I try to use MAG3110 sensor with an arduino due board.

I have a problem when i want to write in the "Ctrl_reg2" register.

I want to write 0x80 in the register but when i read it (just to verify), the register value is 0x00...

I haven't this issue with ctrl_reg1.

Here ou can see the writing code :

       Wire.beginTransmission(MAG_ADDR);   // transmit to device 0x0E

       Wire.write(0x10);                   // ctrl register1

       Wire.write(0x00);                   // Standby

       Wire.endTransmission();             // stop transmitting

       delay(15);

       Wire.beginTransmission(MAG_ADDR);   // transmit to device 0x0E

       Wire.write(0x11);                   // ctrl register2

       Wire.write(0x80);                  // send 0x80, enable auto resets

       Wire.endTransmission();             // stop transmitting

Is there any special things to do with this register ?

Many thanks for the help.

标签 (1)
0 项奖励
回复
4 回复数

1,543 次查看
nicolasdecroze
Contributor I

hi Tomas,

I'm really sorry for late reply but i had a big issue on another project so i hadn't a lot of time...

you  can see below my Arduino source code :

I can see if there is a mistake...

Many thanks for your help.

regards,

Nicolas.

#include <Wire.h>

#define MAG_ADDR  0x0E        // 7-bit address for the MAG3110, doesn't change

void setup()

{

  pinMode(38, INPUT);

  Serial.begin(115200);       // start serial for output

  Wire.begin();               // join i2c bus (address optional for master)

  config();                   // turn the MAG3110 on

}

void loop()

{

  if (digitalRead(38) == HIGH){

      print_values();

  }

}

void config(void)

  Wire.beginTransmission(MAG_ADDR);   // transmit to device 0x0E

  Wire.write(0x10);                   // ctrl register1

  Wire.write(0x00);                   // Standby

  Wire.endTransmission();             // stop transmitting

  delay(15);

  Wire.beginTransmission(MAG_ADDR);   // transmit to device 0x0E

  Wire.write(0x11);                   // ctrl register2

  Wire.write(0x80);                  // send 0x80, enable auto resets

  Wire.endTransmission();             // stop transmitting

  delay(15);

 

  Wire.beginTransmission(MAG_ADDR);   // transmit to device 0x0E

  Wire.write(0x11);                   // ctrl register2

  Wire.write(0x30);                  // send 0x80, enable auto resets

  Wire.endTransmission();             // stop transmitting

 

  delay(15);

  Wire.beginTransmission(MAG_ADDR);   // transmit to device 0x0E

  Wire.write(0x10);                   // ctrl register1

  Wire.write(0xC9);                   // send 0x01, active mode

  Wire.endTransmission();             // stop transmitting

}

void print_values(void)

{

  int LSB_MASK = 0x00FF;

    Serial.write(0x01);

    int16_t X_T = readx();

    Serial.write(X_T>>8);             // MSB

    Serial.write(X_T & LSB_MASK);     // LSB

    int16_t Y_T = ready();

    Serial.write(Y_T>>8);             // MSB

    Serial.write(Y_T & LSB_MASK);     // LSB

    int16_t Z_T = readz(); 

    Serial.write(Z_T>>8);             // MSB

    Serial.write(Z_T & LSB_MASK);     // LSB

    Serial.write(0x02);

}

//////////////////////////////// Read X /////////////////////////////////////

int16_t readx(void)

{

  byte xl = 0;

  byte xh = 0;                      // define the MSB and LSB

  int16_t xout = 0;

 

  Wire.beginTransmission(MAG_ADDR); // transmit to device 0x0E

  Wire.write(0x01);                 // x MSB reg

  Wire.endTransmission();           // stop transmitting

  delayMicroseconds(2);             // needs at least 1.3us free time between start and stop

 

  Wire.requestFrom(MAG_ADDR, 1);    // request 1 byte

 

  while(Wire.available())           // slave may send less than requested

  {

    xh = Wire.read();               // receive the byte

  }

 

  delayMicroseconds(2);             // needs at least 1.3us free time between start and stop

 

  Wire.beginTransmission(MAG_ADDR); // transmit to device 0x0E

  Wire.write(0x02);                 // x LSB reg

  Wire.endTransmission();           // stop transmitting

  delayMicroseconds(2);             // needs at least 1.3us free time between start and stop

 

  Wire.requestFrom(MAG_ADDR, 1);    // request 1 byte

 

  while(Wire.available())           // slave may send less than requested

  {

    xl = Wire.read();               // receive the byte

  }

  //xl = 0;                           // Ici on met le lsb à 0 pour éviter les fluctuations

  xout = (xl|(xh << 8));            // concatenate the MSB and LSB

  return xout;

}

//////////////////////////////// Read Y /////////////////////////////////////

int16_t ready(void)

{

  byte yl = 0;

  byte yh = 0;                   // define the MSB and LSB

  int16_t yout = 0;

 

  Wire.beginTransmission(MAG_ADDR);     // transmit to device 0x0E

  Wire.write(0x03);                     // y MSB reg

  Wire.endTransmission();               // stop transmitting

  delayMicroseconds(2);                 // needs at least 1.3us free time between start and stop

 

  Wire.requestFrom(MAG_ADDR, 1);        // request 1 byte

 

  while(Wire.available())               // slave may send less than requested

  {

    yh = Wire.read();                   // receive the byte

  }

 

  delayMicroseconds(2);                 // needs at least 1.3us free time between start and stop

 

  Wire.beginTransmission(MAG_ADDR);     // transmit to device 0x0E

  Wire.write(0x04);                     // y LSB reg

  Wire.endTransmission();               // stop transmitting

  delayMicroseconds(2);                 // needs at least 1.3us free time between start and stop

 

  Wire.requestFrom(MAG_ADDR, 1);        // request 1 byte

 

  while(Wire.available())               // slave may send less than requested

  {

    yl = Wire.read();                   // receive the byte

  }

  //yl = 0;                               // Ici on met le lsb à 0 pour éviter les fluctuations

  yout = (yl|(yh << 8));                // concatenate the MSB and LSB

 

  return yout;

}

//////////////////////////////// Read Z /////////////////////////////////////

int16_t readz(void)

{

  byte zl = 0;

  byte zh = 0;                   // define the MSB and LSB

  int16_t zout = 0;

 

  Wire.beginTransmission(MAG_ADDR);     // transmit to device 0x0E

  Wire.write(0x05);                     // z MSB reg

  Wire.endTransmission();               // stop transmitting

  delayMicroseconds(2);                 // needs at least 1.3us free time between start and stop

 

  Wire.requestFrom(MAG_ADDR, 1);        // request 1 byte

 

  while(Wire.available())               // slave may send less than requested

  {

    zh = Wire.read();                   // receive the byte

  }

 

  delayMicroseconds(2);                 // needs at least 1.3us free time between start and stop

 

  Wire.beginTransmission(MAG_ADDR);     // transmit to device 0x0E

  Wire.write(0x06);                     // z LSB reg

  Wire.endTransmission();               // stop transmitting

  delayMicroseconds(2);                 // needs at least 1.3us free time between start and stop

 

  Wire.requestFrom(MAG_ADDR, 1);        // request 1 byte

 

  while(Wire.available())               // slave may send less than requested

  {

    zl = Wire.read();                   // receive the byte

  }

  //zl = 0;                               // Ici on met le lsb à 0 pour éviter les fluctuations

  zout = (zl|(zh << 8));                // concatenate the MSB and LSB

 

  return zout;

}

//////////////////////////////// Read CTRL_REG_2 /////////////////////////////////////

byte readctrl2(void)

{

  byte CTRL2;                   // define the MSB and LSB

  Wire.beginTransmission(MAG_ADDR);     // transmit to device 0x0E

  Wire.write(0x11);                     // z MSB reg

  Wire.endTransmission();               // stop transmitting

  delayMicroseconds(2);                 // needs at least 1.3us free time between start and stop

  Wire.requestFrom(MAG_ADDR, 1);        // request 1 byte

 

  while(Wire.available())               // slave may send less than requested

  {

    CTRL2 = Wire.read();                   // receive the byte

  }

 

  return CTRL2;

}

//////////////////////////////// Read CTRL_REG_1 /////////////////////////////////////

byte readctrl1(void)

{

  byte CTRL1;                   // define the MSB and LSB

  Wire.beginTransmission(MAG_ADDR);     // transmit to device 0x0E

  Wire.write(0x10);                     // z MSB reg

  Wire.endTransmission();               // stop transmitting

  delayMicroseconds(2);                 // needs at least 1.3us free time between start and stop

  Wire.requestFrom(MAG_ADDR, 1);        // request 1 byte

   

  while(Wire.available())               // slave may send less than requested

  {

    CTRL1 = Wire.read();                   // receive the byte

  }

 

  return CTRL1;

}

0 项奖励
回复

1,543 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Nicolas,

This is correct behaviour, the AUTO_MRST_EN is a write-only bit and always reads back as 0.

pastedImage_3.png

Let me know if you have any other questions.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 项奖励
回复

1,543 次查看
nicolasdecroze
Contributor I

hi Tomas,

Sorry for late reply, i was in vacation :smileyhappy:

Many thanks for your help !

However i have one more question :

If RAW bit is 1, output data should be beetween -20000 and +20000 is that right?

Because when i put this bit to 1, output values are still beetween -32768 and +32768... is that normal ? or i have an issue in my software?

Regards,

Nicolas

0 项奖励
回复

1,543 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Nicolas,

Having such big values is not normal, unless the device is exposed to strong magnetic fields. Could you please share here your source code and raw values you read from registers 0x01 – 0x06? There may be a problem with converting raw values to signed 16-bit numbers or with incorrect interpreting on output device (if used).

Regards,

Tomas

0 项奖励
回复