FXOS8700CQ is not generating Data ready interrupt on INT1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FXOS8700CQ is not generating Data ready interrupt on INT1

1,529 Views
chandra010
Contributor I

Hi,

I am using Hexiwear development kit. I have configured FXOS8700CQ to generate Data ready interrupt on INT1 (PTC1). But the INT1 interrupt never triggered. FXOS8700CQ configuration is mentioned below. Please let me know, am i missing some thing?

fxos_status_t FXOS_Init( handleFXOS_t* fxosHandle, const settingsFXOS_t* fxosSettings
)
{
/**
* initialize intern structures,
* which will be used from now on
*/

uint8_t chip_ID = 0x00;
uint8_t tmp[1] = {0};

memcpy( (void*)&self, (void*)fxosHandle, sizeof(self) );
memcpy( (void*)&settings, (void*)fxosSettings, sizeof(settings) );

statusI2C_t
status = I2C_Init( &(self.protocol), settings.address, settings.baudRate_kbps );

if ( STATUS_I2C_SUCCESS != status )
{
return status;
}

else
{
statusI2C_t
devStatus = STATUS_I2C_SUCCESS;

devStatus |= I2C_ReadReg( &(self.protocol), WHO_AM_I_REG, &chip_ID);

if(kFXOS_WHO_AM_I_Device_ID == chip_ID)
{

/** go to standby */
devStatus |= I2C_ReadReg(&(self.protocol), FXOS_CTRL_REG1, tmp);

devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG1, tmp[0] & (uint8_t)~ACTIVE_MASK);

devStatus |= I2C_ReadReg(&(self.protocol), FXOS_CTRL_REG1, tmp);
if ((tmp[0] & ACTIVE_MASK) == ACTIVE_MASK)
{
catch( CATCH_I2C );
}

devStatus |= I2C_WriteReg(&(self.protocol), F_SETUP_REG, F_MODE_DISABLED); // Disable the FIFO
devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG2, MOD_HIGH_RES); // /* enable auto-sleep, low power in sleep, high res in wake */

devStatus |= I2C_WriteReg(&(self.protocol), FXOS_M_CTRL_REG1, (M_RST_MASK | M_OSR_MASK | M_HMS_MASK));
devStatus |= I2C_WriteReg(&(self.protocol), FXOS_M_CTRL_REG2, (M_HYB_AUTOINC_MASK));

devStatus |= I2C_WriteReg(&(self.protocol), XYZ_DATA_CFG_REG, FULL_SCALE_4G); // +/-4g range with 0.244mg/LSB

devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG4, 0x01); // Enable DRDY interrupt
devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG5, INT_CFG_DRDY_MASK);
devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG3, WAKE_FF_MT_MASK);
devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG1, HYB_ASLP_RATE_0_8HZ | HYB_DATA_RATE_100HZ | ACTIVE_MASK);

devStatus |= I2C_ReadReg(&(self.protocol), FXOS_CTRL_REG1, tmp);

if ((tmp[0] & ACTIVE_MASK) != ACTIVE_MASK)
{
catch( CATCH_I2C );
}


if ( STATUS_I2C_SUCCESS != devStatus )
{
catch( CATCH_I2C );
}

}

return devStatus;
}
}

//Interrupt configuration

/** create basic tasks */
status |= HostInterface_Init();

SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK; // Turn on clock to Port C module

PORTC_PCR1 |= (0|PORT_PCR_ISF_MASK | 

PORT_PCR_MUX(0x1) | 

PORT_PCR_IRQC(0xA)); // PC1 is configured for falling edge interrupts

//Enable PORTC interrupt on NVIC
NVIC_SetPriority( PORTC_IRQn, HEXIWEAR_TAP_IRQ_PRIO);

Thanks,

J. Chandra Sekhar

0 Kudos
Reply
5 Replies

1,518 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Chandra,

I hope all is great with you. Thank you for using the NXP communities.

In this case, I highly recommend using the following bare metal project as a reference for your design:

FXOS8700CQ - Bare metal example project

I hope this information helps.

Regards,

David

0 Kudos
Reply

1,484 Views
chandra010
Contributor I

Hi,

Thanks for your response.

I have checked the code and configured similarly in my Hexiwear board. But still the same, FXOS8700CQ sensor is not generating interrupt.  

const gpio_input_pin_user_config_t Acc_cfg[] = {
{
.pinName = ACC_INT1,
.config.isPullEnable = false,
.config.pullSelect = kPortPullDown,
.config.isPassiveFilterEnabled = false,
.config.isDigitalFilterEnabled = false,
.config.interrupt = kPortIntDisabled
},
{
.pinName = ACC_INT2,
.config.isPullEnable = false,
.config.pullSelect = kPortPullDown,
.config.isPassiveFilterEnabled = false,
.config.isDigitalFilterEnabled = false,
.config.interrupt = kPortIntDisabled
},
{
.pinName = GPIO_PINS_OUT_OF_RANGE,
}
};

//Configured Pin 1 of PORTC as input

GPIO_DRV_Init( Acc_cfg, NULL ); 

//Sensor configuration

devStatus |= I2C_ReadReg( &(self.protocol), WHO_AM_I_REG, &chip_ID);

if(kFXOS_WHO_AM_I_Device_ID == chip_ID)
{
/** go to standby */
FXOS_GotoStandby();

devStatus |= I2C_ReadReg(&(self.protocol), FXOS_CTRL_REG1, tmp);

devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG1, tmp[0] & (uint8_t)~ACTIVE_MASK);

devStatus |= I2C_ReadReg(&(self.protocol), FXOS_CTRL_REG1, tmp);
if ((tmp[0] & ACTIVE_MASK) == ACTIVE_MASK)
{
catch( CATCH_I2C );
}

devStatus |= I2C_WriteReg(&(self.protocol), XYZ_DATA_CFG_REG, FULL_SCALE_2G); // +/-2g range with 0.244mg/LSB

devStatus |= I2C_WriteReg(&(self.protocol), FXOS_M_CTRL_REG1, (0x1F)); // Hybrid mode (accelerometer + magnetometer), max OSR
devStatus |= I2C_WriteReg(&(self.protocol), FXOS_M_CTRL_REG2, 0x20); // M_OUT_X_MSB register 0x33 follows the OUT_Z_LSB register 0x06 (used for burst read)


devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG2, 0x02); // High Resolution mode
devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG3, 0x00); // Push-pull, active low

devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG4, 0x01); // Enable DRDY interrupt
devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG5, 0x01); // DRDY interrupt routed to INT1 - PTC1

devStatus |= I2C_WriteReg(&(self.protocol), FXOS_CTRL_REG1, 0x35); // ODR = 3.125Hz, Reduced noise, Active mode

FXOS_SetActive();

if ( STATUS_I2C_SUCCESS != devStatus )
{
catch( CATCH_I2C );
}

}

//Interrupt handler

void PORTC_IRQHandler(void)
{
PORT_HAL_ClearPortIntFlag(PORTC_BASE_PTR);
/** Write your code here ... */
/* Unblock the task by releasing the semaphore. */
portBASE_TYPE taskToWake = pdFALSE;

if (pdTRUE==xSemaphoreGiveFromISR(xReadRawDataSemaphore, &taskToWake))
{
FXOS8700CQ_DataReady = 1;
if (pdTRUE == taskToWake)
{
vPortYieldFromISR();
}
}
}

//Task to read data from sensor

void ReadRawData(task_param_t param)
{

xReadRawDataSemaphore = xSemaphoreCreateBinary();

if( xReadRawDataSemaphore == NULL )
{
configASSERT(0);
}

for(;;)
{
/*Block waiting for the semaphore to become available. */
if( xSemaphoreTake( xReadRawDataSemaphore, LONG_TIME ) == pdTRUE )
{
if(FXOS8700CQ_DataReady)
{
FXOS8700CQ_DataReady = 0;

FXOS_ReadRawData(&AccelMagData[0]);
}

vPortYieldFromISR();
}

}

}

Trying this from few days, but no luck. Request your support.

 

Thanks,

J. Chandra Sekhar

 

 

 

 

 

 

 

0 Kudos
Reply

1,452 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Chandra,

Thank you for using the community. 

Your device configuration seems correct. I just want to recommend applying a reset to all registers before device the configuration.

diazmarin09_0-1678823128560.png

Could you please make sure the INT1 pin is connected to your MCU/MPU input pin? Is your input pin configured for falling edge interrupts?

Regards,

David

0 Kudos
Reply

1,434 Views
chandra010
Contributor I

Hi,

To perform Soft reset, i have used below code. But this command resulting the STATUS_I2C_ERROR.

fxos_status_t FXOS_SoftReset()
{
statusI2C_t
i2cStatus = I2C_WriteReg( &(self.protocol), FXOS_CTRL_REG2, RST_MASK );

if ( STATUS_I2C_SUCCESS != i2cStatus )
{
return STATUS_FXOS_PROTOCOL_ERROR;
}
else
{
return STATUS_FXOS_SUCCESS;
}
}

 

Thanks,

J. Chandra Sekhar

0 Kudos
Reply

1,427 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Chandra,

I do recommend performing the reset just writing 0x40 to the CTRL_REG2 register.

diazmarin09_1-1679078726099.png

Could you please make sure the INT1 pin is connected to your MCU/MPU input pin? Is your input pin configured for falling edge interrupts?               

Regards,

David

0 Kudos
Reply