FXOS8700 stops updating value after a while

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FXOS8700 stops updating value after a while

2,182 Views
rens1
Contributor I

hello everyone,

Currently i'm working with the BRKT-STBC-AGM01  BREAKOUT BOARD. Where i'm communicating with a FXOS8700cq chip through I2C with my Atxmega microcontroller.

I have set up the IC to getting only magnetic values on 200Hz samples rate.

But after a while i don't new data from the chip anymore. I thought that it might have been the sleep mode. But i disabled that one. As far as i know. Is there something else that i overlooked?

Hereby my setup code :

        TWI_Write(FXOS8700CQ_SLAVE_ADDR,FXOS_CTRL_REG1,0x00);

        TWI_Write(FXOS8700CQ_SLAVE_ADDR,FXOS_CTRL_REG2,0x09);

        //TWI_Write(FXOS8700CQ_SLAVE_ADDR,FXOS_XYZ_DATA_CFG,0x00);

        TWI_Write(FXOS8700CQ_SLAVE_ADDR,FXOS_M_CTRL_REG1,0x05);

        TWI_Write(FXOS8700CQ_SLAVE_ADDR,FXOS_M_CTRL_REG2,0x49);

        TWI_Write(FXOS8700CQ_SLAVE_ADDR,FXOS_M_CTRL_REG3,0xA0);

        TWI_Write(FXOS8700CQ_SLAVE_ADDR,FXOS_CTRL_REG1,0x15);

Did i forget something with the initialisation?

Thanks in advance,

Labels (1)
0 Kudos
Reply
3 Replies

1,253 Views
david_diaz
NXP Employee
NXP Employee

Hello Rens,

Please be aware about the M_CTRL_REG2. You do not need to set the auto-increment mode due to you are using the magnetometer mode only.

You may use the following configuration in order to initialize the FXOS8700QC:

     I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, CTRL_REG2, 0x40);          // Reset all registers to POR values, Standby mode

       Delay();        // ~1ms delay

     I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, XYZ_DATA_CFG_REG, 0x00);   // +/-2g range with 0.244mg/LSB  

       I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, M_CTRL_REG1, 0x1D);        // Magnetometer mode, max OSR

     I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, CTRL_REG2, 0x02);          // High Resolution mode

     I2C_WriteRegister(FXOS8700CQ_I2C_ADDRESS, CTRL_REG1, 0x15);          // ODR = 200Hz, Reduced noise, Active mode  

Please let me know if this configuration helps.

In case it is useful for you, you may refer to the FX0S87OOCQ - Bare metal example project.

https://community.freescale.com/docs/DOC-101073

I hope this information will be useful for you.

If I misunderstood your question or you still have concerns, feel free to let me know.  I will be glad to help.

Have a great day.

David Diaz.

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply

1,253 Views
rens1
Contributor I

thank for the reply,

Have been away for a bit. That's why i couldn't reply earlier. But it seems with the setting you send to me. The same problems occurs. After a while it just stops giving new data. And only gives Zero's back from the registers. Could it be i'm missing something or is the chip maybe broken ?

Greetings,

Rens

0 Kudos
Reply

1,253 Views
rens1
Contributor I

I just found out that the magnetometer goes in to standby mode at a random moment.

With every sample i take i read that Sysmod register to see if the chip is still active. And there it stated that it had gone into standby mode.

Is there something that i forgot that could cause the chip to go into standby more or could it really be broken? I do have the reset line set to ground.

Greetings,

Rens

0 Kudos
Reply