FXLS8962 moves slowly and cannot trigger interrupt. How can I solve this problem?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FXLS8962 moves slowly and cannot trigger interrupt. How can I solve this problem?

4,115件の閲覧回数
qiuquanfeng
Contributor II

The motion sensor moves horizontally or vertically on the table without interruption. When 2g and 16g are configured, or the sampling period is configured with different values, no interruption can be generated in the process of slow movement. May I ask how to improve the sensitivity to solve this problem? The attachment is the configuration file of different parameters of 8962, may I ask whether the configuration file needs to be changed? Thank you.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

4,091件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

并没有看到您放的附件!

客户的信息能说明一下吗?谢谢!

0 件の賞賛
返信

4,086件の閲覧回数
qiuquanfeng
Contributor II

您好!客户是steel-mate,问题出现的背景和终端客户反馈,把钥匙放入口袋或者拿着缓慢移动的时候,并不能唤醒系统。客户拿回来设备进行测试,现象是配置参数为4G、8G、16G发现缓慢移动的时候,接上逻辑分析仪是发现没有中断产生。附件是不同参数配置代码文件,您帮忙看下,感谢支持!

0 件の賞賛
返信

4,023件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Had escalated to PAE side,please wait for response!

 

0 件の賞賛
返信