About MM9Z1638 Interrupt question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About MM9Z1638 Interrupt question

2,284 Views
dws
Contributor III

Hi all,

I come across Dead loop when the program come into interrupt D2DINTCH3.

The preconditon is that I connect with nothing only a bare board.

pastedImage_1.png

Could you help me clarify the question?

Thank you!

Dawei

Labels (1)
0 Kudos
Reply
1 Reply

1,616 Views
darioarias
NXP Employee
NXP Employee

Hi,

Thank you for writing

It is rather difficult to tell why you are coming to a Dead Loop by just looking to a section of your code, however I can recommend you to take a look to the following attached application note which talks a bit about the Die-to-Die interface, and also I'd like to share with you an example code for this part that shows how to use the interrupts where the D2D is included.

Regards,

Dario

0 Kudos
Reply