About MM9Z1638 Interrupt question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About MM9Z1638 Interrupt question

2,186件の閲覧回数
dws
Contributor III

Hi all,

I come across Dead loop when the program come into interrupt D2DINTCH3.

The preconditon is that I connect with nothing only a bare board.

pastedImage_1.png

Could you help me clarify the question?

Thank you!

Dawei

ラベル(1)
0 件の賞賛
返信
1 返信

1,518件の閲覧回数
darioarias
NXP Employee
NXP Employee

Hi,

Thank you for writing

It is rather difficult to tell why you are coming to a Dead Loop by just looking to a section of your code, however I can recommend you to take a look to the following attached application note which talks a bit about the Die-to-Die interface, and also I'd like to share with you an example code for this part that shows how to use the interrupts where the D2D is included.

Regards,

Dario

0 件の賞賛
返信