87E RF send demo

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

87E RF send demo

1,483 次查看
xiaohui200808
Contributor III

Hello:#

        there are two kinds of send RF :1  RF DATA buffer  mode,2 MCU Direct mode.I want to use MCU Direct mode.Is there any demo code ?

        I find some code in    FXTH87EDRM.pdf   ,but it do not work .

thank you!

 

标签 (1)
0 项奖励
回复
1 回复

1,416 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Xiaohui,

I included datasheet extracts giving more information on the MCU direct mode below. But in summary the following must be done:

  1. Configure PLLCR3_CODE = 1 to configure direct mode;
  2. Configure RFCR2_SEND = 1 to enable the RF output;
  3. Wait for RF output stage to be stable by monitoring RFCR7_RCTS bit;
  4. Control the RF signal to be high state or low state with RFCR3_DATA bit.

MCU Direct Mode.jpg

Table 77.jpg

I hope it helps.

Best regards,

Tomas

0 项奖励
回复