Secure Provisioning SDK (SPSDK)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Secure Provisioning SDK (SPSDK)

Secure Provisioning SDK (SPSDK) is an open-source development kit with its source code released on Github and PyPI. It contains a set of API modules for custom production tool development which requires more advanced secure provisioning flow. SPSDK enables communication with NXP’s microcontrollers for security features configuration, debug authentication, generation of Secure Binary (SB) images, trust provisioning and secure programming, etc.

Where to start?

  • Visit SPSDK landing page for the latest document and software on Github and PyPI.
  • Latest news? View “Announcement” label below
  • Get help or report issues? Visit Github. We centralize code release and support on Github.
Labels

Discussions

Sort by:
We are excited to announce the release of Secure Provisioning SDK (SPSDK) 3.6.0 Please note this release is a new generation of SPSDK and it is NOT backward compatible to 2.x versions.  A migration guide is provided below: ⭐What's NEW: https://spsdk.readthedocs.io/en/latest/release_notes.html ⚠️Migration Guide: https://spsdk.readthedocs.io/en/latest/migration_guide.html 📦Supported Devices: https://spsdk.readthedocs.io/en/latest/devices_list.html 👇More details: Github PyPi Documentation   SPSDK Plugins 3.6.0: Github (Plugins) PyPi (Plugins) Note: nxp-codecheck was moved to separated repository bellow: SPSDK Codecheck 0.3.16: GitHub: https://github.com/nxp-mcuxpresso/nxp-codecheck PyPi: https://pypi.org/project/nxp-codecheck/   Starting from SPSDK 3.2.0 and onwards, Restricted Data Package is no longer needed.
View full article
We are excited to announce the release of Secure Provisioning SDK (SPSDK) 3.13.0 🆕 New device support MCXC353, MCXC352 MCXN526T MIMXRT1183, MIMXRT118D ✨ Key new features nxpdebugmbox: new tool execute command, Debug Authentication Response export, improved debug connection diagnostics, and probe discovery without a mandatory family filter. Debug probes: ARM ADIv6 (CoreSight 600 / DPv3) support with automatic ADI-version detection and MEM-AP/debug-mailbox discovery. nxpimage: DevHSM SRK-set support plus secondary-image tables and parallel AHAB verification for MIMXRT266x devices. nxpele: new forward-boot-crypto command, HSE core reset/status support, and second Cortex-M7 core support for MCXE327 and MCXE32B. nxpcrypto: new --fuse-script option for rot calculate-hash to generate device-specific RoT fuse scripts where supported. Migration checks: new SPSDK_DEPRECATED_STRICT environment variable to report deprecated register aliases and schema properties as errors. For more details: Release Notes Supported Devices Github PyPi Documentation   SPSDK Plugins: Github (Plugins) PyPi (Plugins)   Note: nxp-codecheck was moved to separated repository bellow: SPSDK Codecheck: GitHub: https://github.com/nxp-mcuxpresso/nxp-codecheck PyPi: https://pypi.org/project/nxp-codecheck/  
View full article
We are pleased to announce the release of Rapid Blhost (RBLHOST) 0.3.0. RBLHOST is a host-side utility for communicating with embedded devices over interfaces such as USB and UART. Built in Rust with a focus on high performance for time-critical applications, it can be seamlessly integrated into systems developed in Python, C, or Rust. Features UART communication with configurable baudrate and timeout I2C communication with configurable slave address USB-HID communication with configurable VID/PID, and selection of one specific device by OS path, serial number or USB topology (port) path when several identical boards are connected Command-line interface compatible with the original blhost tool Batch command files executed sequentially in one process and one device session Python bindings for integration with other tools C/C++ bindings supported (UART, I2C and USB-HID, see MBoot C Bindings) ... and more!  Check this out! 🐙 GitHub: https://github.com/nxp-mcuxpresso/rblhost 📦 Crates.io: https://crates.io/crates/rblhost
View full article
We are excited to announce the release of Secure Provisioning SDK (SPSDK) 3.4.0 Please note this release is a new generation of SPSDK and it is NOT backward compatible to 2.x versions.  A migration guide is provided below: ⭐What's NEW: https://spsdk.readthedocs.io/en/latest/release_notes.html ⚠️Migration Guide: https://spsdk.readthedocs.io/en/latest/migration_guide.html 📦Supported Devices: https://spsdk.readthedocs.io/en/latest/devices_list.html 👇More details: Github PyPi Documentation   SPSDK Plugins 3.4.0: Github (Plugins) PyPi (Plugins) Note: nxp-codecheck was moved to separated repository bellow: SPSDK Codecheck 0.3.14: GitHub: https://github.com/nxp-mcuxpresso/nxp-codecheck PyPi: https://pypi.org/project/nxp-codecheck/   Starting from SPSDK 3.2.0 and onwards, Restricted Data Package is no longer needed.
View full article
If you are using SPSDK 3.1, you may probably need to access the Restricted Data Package.  Here is the new location that you can find this package on SPSDK page: Login to nxp.com.  Go to "Downloads" section, then choose the "Secure" radio button on the left.  You should see the Restricted Data Package.   You may be asked to fill out a form for additional access if you haven't done it before.  After that, our system will check if we have a valid NDA with your company, then grant you the access to download the package. Note: The Restricted Data Package is no longer needed from SPSDK v3.2 and onwards. Restricted Data Package new location
View full article
We are excited to announce the release of Secure Provisioning SDK (SPSDK) 3.3.0 Please note this release is a new generation of SPSDK and it is NOT backward compatible to 2.x versions.  A migration guide is provided below: ⭐What's NEW: https://spsdk.readthedocs.io/en/latest/release_notes.html ⚠️Migration Guide: https://spsdk.readthedocs.io/en/latest/migration_guide.html 📦Supported Devices: https://spsdk.readthedocs.io/en/latest/devices_list.html 👇More details: Github PyPi Documentation   SPSDK Plugins 3.3.0: Github (Plugins) PyPi (Plugins)   Starting from SPSDK 3.2.0 and onwards, Restricted Data Package is no longer needed.
View full article
What is Rapid Blhost (RBLHOST)? RBLHOST is a command-line utility provides MCU bootloader library used on host computer/processor for issuing commands to NXP MCUs via UART and I2C.  Its command-line interface is compatible with the original blhost tool for image programming. It is designed to deliver high performance for time-critical applications and enables seamless integration into systems developed in Python, C, or Rust—the core language used for this project.  More information about RBLHOST can be found below:   Rapid Blhost (RBLHOST) 0.1.0: GitHub: https://github.com/nxp-mcuxpresso/rblhost Documentation: https://crates.io/crates/rblhost
View full article
We are excited to annouce the release of Secure Provisioning SDK (SPSDK) 3.2.0 Please note this release is a new generation of SPSDK and it is NOT backward compatible to 2.x versions.  A migration guide is provided below: ⭐What's NEW: https://spsdk.readthedocs.io/en/latest/release_notes.html ⚠️Migration Guide: https://spsdk.readthedocs.io/en/latest/migration_guide.html 📦Supported Devices: https://spsdk.readthedocs.io/en/latest/devices_list.html 👇More details: Github PyPi Documentation   SPSDK Plugins 3.2.0: Github (Plugins) PyPi (Plugins)   Starting from SPSDK 3.2.0 and onwards, Restricted Data Package is no longer needed.  
View full article
We are excited to annouce the release of Secure Provisioning SDK (SPSDK) 3.1 Please note this release is a new generation of SPSDK and it is NOT backward compatible to 2.x versions.  A migration guide is provided below: ⭐What's NEW: https://spsdk.readthedocs.io/en/latest/release_notes.html ⚠️Migration Guide: https://spsdk.readthedocs.io/en/latest/migration_guide.html 📦Supported Devices: https://spsdk.readthedocs.io/en/latest/devices_list.html 👇More details: Github PyPi Documentation   SPSDK Plugins 3.1: Github (Plugins) PyPi (Plugins)   Restricted Data Package for SPSDK 3.1: Please note that the package uses an LA_OPT license. Package will be located in the Download section.
View full article
We are excited to annouce the release of Secure Provisioning SDK (SPSDK) 3.0.0 Please note this release is a new generation of SPSDK and it is NOT backward compatible to previous versions.  A migration guide  is provided below: ⭐What's NEW: https://spsdk.readthedocs.io/en/latest/release_notes.html ⚠️Migration Guide: https://spsdk.readthedocs.io/en/latest/migration_guide.html 📦Supported Devices: https://spsdk.readthedocs.io/en/latest/devices_list.html 👇More details: Github PyPi Documentation   SPSDK Plugins 3.0.0: Github (Plugins) PyPi (Plugins)   Restricted Data Package for SPSDK 3.0.0: Please note that the package uses an LA_OPT license. Package will be located in the Download section.  
View full article
SPSDK v2.6.1 is now available for download. This release includes several bug fixes as detailed in the release notes. No changes on Plugins and Restricted Data Package. 
View full article
SPSDK v2.6 is now available for download This release delivers: The support of MCX W23x, i.MX 943, i.MX 8ULP Add possibility to save OEM app config Support of set CRP in lpcprog Add optional parameter to repeat the command several times if fails Support BCA and FCF configuration for MCX Cxxx Implement Key Import signed message Add support for RSA in DAT on i.MX RT118x   SPSDK Plugins 0.5.0: The plugins update: Checkers improvements GitHub: https://github.com/nxp-mcuxpresso/spsdk_plugins PyPi: https://pypi.org/search/?q=spsdk&o=   Restricted Data Package for SPSDK 2.6: The data contains: MCX A163, MCX A164, MCX L253, MCX L254, MCX L255, i.MX 91,  i.MX 95 Please note that the package uses an LA_OPT license. Package will be located in the Download section: https://www.nxp.com/design/design-center/software/development-software/secure-provisioning-sdk-spsdk:SPSDK
View full article
SPSDK v2.5 is now available for download This release delivers: New devices supported: i.MX RT735S and i.MX RT758S i.MX RT1043 and i.MX RT1046 MCX A13x variants KW47xx and MCX W72x devices EdgeLock 2GO: enablement for i.MX 93 New Fuse Tool: nxpfuses for handling operations with fuses Python 3.13 support Drop pyocd  and replace by spsdk-mcu-link and spsdk-pyocd   SPSDK Plugins 0.4.0: The plugins update: MCU-Link debug probe support plugin for NXP LPC-Link/MCU-Link hardware debug probes. GitHub: https://github.com/nxp-mcuxpresso/spsdk_plugins PyPi: https://pypi.org/search/?q=spsdk&o=   Restricted Data Package for SPSDK 2.5: The delivery to the web is currently in process and will be available soon. The data contains: MCX A163, MCX A164, MCX L253, MCX L254, MCX L255, i.MX 91, i.MX 943, i.MX95 Please note that the package uses an LA_OPT license. Package will be located in the Download section: https://www.nxp.com/design/design-center/software/development-software/secure-provisioning-sdk-spsdk:SPSDK
View full article
SPSDK v2.3 is now available for download This release brings new features for i.MX 93 and i.MX 95: Support for signing and encryption of existing AHAB (nxpimage ahab sign) Support for new AHAB container with PQC format version 2 Command for creating the PKI tree (nxpcrypto pki-tree) Support for i.MX95 DAT A0/A1/B0 revisions SPSDK integrates UUU with and brings python wrapper for libuuu https://pypi.org/project/libuuu/ New tool nxpuuu for programming of devices from SPSDK Support for nxpele over fastboot The latest changes are shown in the release notes  
View full article
SPSDK v2.2.1 is now available for download New features include: Added CAN support for blhost Added EdgeLock 2Go support for MWCT2x12, MWCT2xD2 and RW61x New plugins available The latest changes are shown in the release notes  
View full article
We have upgraded SPSDK to 2.0.1 which includes a large scale of changes: elftosb will be replaced by nxpimage nxpcertgen and nxpkeygen will be replaced by nxpcrypto select appropriate family will be done using: -f/–family parameter move towards options for all parameters with an exception to BLHost removal of crypto backends extend dedicated spsdk.crypto module - serve as the de-facto backend of SPSDK module level imports via init files
View full article
We plan to upgrade SPSDK to 2.0 in the next release which includes a large scale of changes.  Customers are suggested to prepare for the changes before the 2.0 release (end of Sept 2023).  Major changes in 2.0 are: elftosb will be replaced by nxpimage nxpcertgen and nxpkeygen will be replaced by nxpcrypto select appropriate family will be done using: -f/–family parameter move towards options for all parameters with an exception to BLHost removal of crypto backends extend dedicated spsdk.crypto module - serve as the de-facto backend of SPSDK module level imports via init files
View full article