send data through MCU connect with a71CH

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

send data through MCU connect with a71CH

2,151件の閲覧回数
phuongph1997
Contributor I

I want to encrypt data use A71CH and send data to cloud . but i found a few topic  said that A71CH could not help with data encrypted or decrypted.  the MCU does this task. is this true ?.

please help me!

タグ(2)
0 件の賞賛
返信
1 返信

2,018件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, your understanding is correct, and you have to use the MCU to encrypt and decrypt the data. The only thing the A71CH can do is key diversification which may help the MCU as any master key could be kept inside the A71CH.


Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信