send data through MCU connect with a71CH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

send data through MCU connect with a71CH

2,234 Views
phuongph1997
Contributor I

I want to encrypt data use A71CH and send data to cloud . but i found a few topic  said that A71CH could not help with data encrypted or decrypted.  the MCU does this task. is this true ?.

please help me!

Tags (2)
0 Kudos
Reply
1 Reply

2,101 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, your understanding is correct, and you have to use the MCU to encrypt and decrypt the data. The only thing the A71CH can do is key diversification which may help the MCU as any master key could be kept inside the A71CH.


Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply