SE050 memory writes, wear leveling?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SE050 memory writes, wear leveling?

ソリューションへジャンプ
2,105件の閲覧回数
deang
Contributor III

Per the datasheet, the SE050 memory reliability is "100 Mio write cycles/25 years".  

What does "Mio" mean?  Is this short for Million?

Also, does the se050 implement any kind of wear leveling?

 

Thanks,

Dean

0 件の賞賛
返信
1 解決策
2,042件の閲覧回数
deang
Contributor III

 @Kan_Li Thanks for the clarification.

Dean

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,048件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

Yes, it is short for Million, and  SE05x implements automatic wear leveling. This is why in the datasheet we only specify one global write endurance, as we are spreading writes automatically over the whole flash of the SE.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,043件の閲覧回数
deang
Contributor III

 @Kan_Li Thanks for the clarification.

Dean

 

0 件の賞賛
返信