SE050 memory writes, wear leveling?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SE050 memory writes, wear leveling?

Jump to solution
2,352 Views
deang
Contributor III

Per the datasheet, the SE050 memory reliability is "100 Mio write cycles/25 years".  

What does "Mio" mean?  Is this short for Million?

Also, does the se050 implement any kind of wear leveling?

 

Thanks,

Dean

0 Kudos
Reply
1 Solution
2,289 Views
deang
Contributor III

 @Kan_Li Thanks for the clarification.

Dean

 

View solution in original post

0 Kudos
Reply
2 Replies
2,295 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @deang ,

 

Yes, it is short for Million, and  SE05x implements automatic wear leveling. This is why in the datasheet we only specify one global write endurance, as we are spreading writes automatically over the whole flash of the SE.

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,289 Views
deang
Contributor III

 @Kan_Li Thanks for the clarification.

Dean

 

0 Kudos
Reply