SE050 error while connecting to GCP from FRDMK64F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SE050 error while connecting to GCP from FRDMK64F

2,864件の閲覧回数
pavankumar_vadh
Contributor I

Getting error: "sss:ERROR:SM_RjctConnect Failed. Status 7002" while connecting to GCP from FRDMK64F following this document (https://www.nxp.com/docs/en/application-note/AN12401-SE050_secure_connection_google_cloud_iot_core.p...) for connecting GCP and FRDMK64F board through SE050

In the step 3.1.1.3 Key Injection, after executing commnand in point 2c: ssscli.exe se05x reset, getting the following error "sss:ERROR:SM_RjctConnect Failed. Status 7002". Find the screenshot for the same in the attachment.

タグ(3)
0 件の賞賛
返信
1 返信

2,727件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi ,

I just followed this app note to the step you specified, it works as expected:

pastedImage_1.png

Did you have any warning/error message in previous steps? and please make sure to the demo board is well connected via the vcom port.

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信