RTD drivers with GCC 6.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTD drivers with GCC 6.3

596 Views
mattiasecchiaro
Contributor I

Dear community,

we have already posted this question a month ago on the S32K product forum, but no answers till now. Hopefully here someone can help.

We are working on a project with:

  • MCU S32K148
  • SDK Version 3.0.3 RTM
  • S32 Design Studio IDE Version 2.2
  • Compiler GCC v6.3
  • non-AUTOSAR environment

We need to evaluate transition from SDK Version 3.0.3 to RTD Drivers Version 1.0.0.

Could we still use our actual GCC version? Or are we forced to change to GCC v9.2 (seems that all examples are with this compiler)?

 

Thanks in advance for the support.

Mattia.

0 Kudos
1 Reply

589 Views
martinkaspar-r3
NXP Employee
NXP Employee

The RTD is tested with compiler version and compiler options as documented in the RTD release notes. Usually the release will work also with other compiler versions and compiler options but this is not tested/validated by NXP.

Note that NXP also provides a paid service to customers (CCT - Customer Compiler Test, done per request from customer) where NXP will run the complete RTD testing/validation as per customer selected compiler version and compiler options.

0 Kudos