Functional Safety implementation example on S32K1xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Functional Safety implementation example on S32K1xx

5,585 Views
wei_w_he
Contributor IV

Dear Officer,

NXP has the Safety manual explaining the methods for implementing the FS feature on S32K1xx, Do NXP has some example (source) code?

Thanks and best regards

He Wei

11 Replies

5,507 Views
oscar_hinojosa
Senior Contributor II

Hello He Wei,

Sorry for the delay, regarding the examples codes; We created an app note that helps to understand the examples and how is implemented each assumption but this is a draft version and is attached to this post, also you can find the examples in this link.

 

Best regards,

Oscar Hinojosa.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

Note:- If this post answers your question, please click the Accept as Solution button.
Thank you!
Best regards,
Oscar Hinojosa.
-

5,401 Views
Matthias_LEHMANN
Contributor III

Hello Oscar,

I'm a bit confused about SM_047 in the S32 Safety Manual. The cookbook says that this assumption is fulfilled if it is ensured that no debugging device is connected (essentially a process barrier, maybe also a physical one). The following sentence states that debugging should be disabled in the field. Is this already achieved by not connecting any debugging devices (i.e. essentially by the first sentence) or does this second sentence imply that an additional HW-barrier is also required? Specifically, the safety manual states that JTAG-TMS should be pulled low. If that's the case however, it looks like it's not possible to programm the controller anymore? We use SWD-DIO to programm the controller during production. Once fully assembled, the controller is in its casing and this interface is physically not accessible anymore. Would that satisfy the assumption, even if JTAG-TMS is not permanently pulled low by a resistor?

Best regards

Matthias

\\// Matthias
0 Kudos

5,434 Views
simoneblink
Contributor II

Hello @oscar_hinojosa,

any update about the examples?

The link is not working.

 

Thank you and regards

0 Kudos

5,481 Views
wei_w_he
Contributor IV

Dear Officer,

I can't log in the below link to get the example code:

https://bitbucket.sw.nxp.com/projects/AAG/repos/s32k1xx_safety_cookbook/browse

Is it still available? Or I didn't get permission to log in that link? Can share the example via other way?

Tks and best regards

He Wei

 

 

 

 

5,507 Views
vishnukumar_n
Contributor II

Hello nxf53698

Thanks a lot for sharing the Draft version.

0 Kudos

5,507 Views
vishnukumar_n
Contributor II

Hello nxf53698

Could you share the link to download this?

0 Kudos

5,507 Views
oscar_hinojosa
Senior Contributor II

Hello,

We are working to finish some examples, now we can share with you an internal draft.

Best regards,

Oscar Hinojosa.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

Note:- If this post answers your question, please click the Accept as Solution button.
Thank you!
Best regards,
Oscar Hinojosa.
-
0 Kudos

5,353 Views
simoneblink
Contributor II

Hello Oscar,

more than a year has passed. Do you have updated examples?

(I neither have the draft version because the link was broken)

 

Thank you and kind regards,

Simone

0 Kudos

5,507 Views
yin_hua
Contributor II

Dear Oscar,

Could you please share me with the examples or post it in NXP community where I can download it.

Thanks in advance for helping

5,507 Views
wei_w_he
Contributor IV

Dear Oscar,

Thanks a lot. May I know where I can get/download this internal draft?

Best regards

He Wei

5,507 Views
liting_zhao
Contributor I

Hello

Can you also share me with the internal draft? Thanks!