FIT without WDOG self test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FIT without WDOG self test

ソリューションへジャンプ
788件の閲覧回数
luca_toso
Contributor II

Hi all

Assuming all the assumptions from the Safety manuals are implemented,

what is the expected FIT for S32K11x when the Watchdog self test is not implemented?

 

K.R.

L.T.

 

0 件の賞賛
1 解決策
781件の閲覧回数
nxf61080
NXP Employee
NXP Employee

Hi LT,

In the current FMEDA, which can be found at the following location (https://community.nxp.com/t5/SafeAssure-NDA-group/MCUs-MPUs-available-Functional-Safety-documents-Sa...), we haven’t claimed the FIT for WDog self-test. If you use WDog self-test, this will be covered: 3.66649E-11[This snap has been taken from S32K118 Core FMEDA]

nxf61080_0-1640061197496.jpeg
Thanks and regards,
Manibha

元の投稿で解決策を見る

0 件の賞賛
1 返信
782件の閲覧回数
nxf61080
NXP Employee
NXP Employee

Hi LT,

In the current FMEDA, which can be found at the following location (https://community.nxp.com/t5/SafeAssure-NDA-group/MCUs-MPUs-available-Functional-Safety-documents-Sa...), we haven’t claimed the FIT for WDog self-test. If you use WDog self-test, this will be covered: 3.66649E-11[This snap has been taken from S32K118 Core FMEDA]

nxf61080_0-1640061197496.jpeg
Thanks and regards,
Manibha

0 件の賞賛