FIT without WDOG self test

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FIT without WDOG self test

跳至解决方案
785 次查看
luca_toso
Contributor II

Hi all

Assuming all the assumptions from the Safety manuals are implemented,

what is the expected FIT for S32K11x when the Watchdog self test is not implemented?

 

K.R.

L.T.

 

0 项奖励
1 解答
778 次查看
nxf61080
NXP Employee
NXP Employee

Hi LT,

In the current FMEDA, which can be found at the following location (https://community.nxp.com/t5/SafeAssure-NDA-group/MCUs-MPUs-available-Functional-Safety-documents-Sa...), we haven’t claimed the FIT for WDog self-test. If you use WDog self-test, this will be covered: 3.66649E-11[This snap has been taken from S32K118 Core FMEDA]

nxf61080_0-1640061197496.jpeg
Thanks and regards,
Manibha

在原帖中查看解决方案

0 项奖励
1 回复
779 次查看
nxf61080
NXP Employee
NXP Employee

Hi LT,

In the current FMEDA, which can be found at the following location (https://community.nxp.com/t5/SafeAssure-NDA-group/MCUs-MPUs-available-Functional-Safety-documents-Sa...), we haven’t claimed the FIT for WDog self-test. If you use WDog self-test, this will be covered: 3.66649E-11[This snap has been taken from S32K118 Core FMEDA]

nxf61080_0-1640061197496.jpeg
Thanks and regards,
Manibha

0 项奖励