ADC Channels for safety integrity functions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC Channels for safety integrity functions

762件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Team,

We received the following question:

In Document Number: S32K1XXSM, Rev. 6, 11/2020 Chapter "5.7.2.3.2.1.1 Implementation details" on page 84 is stated that:
The following S32K1xx hardware elements can be used for the safety integrity functions:
• Analog input channels ADC0_SE[0:3], ADC0_SE[6:7] and ADC0_SE[10:15]
• Analog input channels AN[11:14] of ADC0_SE[4:5], ADC1_SE[8:9] and ADC1_SE[14:15] (shared channels)
• Analog input channels ADC1_SE[0:7] and ADC1_SE[10:13]

My question is why ADC0_SE[8:9] are excluded in this list. They are suitable for dual read inputs (5.7.2.3.1.2 Double read analog inputs) so it is not clear for me why they should not be usable as single read inputs.

Please clarify this topic, as we use this channels as single read analog inputs.

Any insights will be appreciated,

 

Regards,

Daniel

0 件の賞賛
2 返答(返信)

730件の閲覧回数
nxf61080
NXP Employee
NXP Employee

Hello Daniel,

We don’t see any issue in using them as single-read analog inputs as long as required recommendations for single-read analog inputs are followed.

Thanks and regards,
Manibha 

737件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello team,

Can you please help to clarify this description?

 

Thank you,

BR, Daniel

 

0 件の賞賛