Question about the error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about the error

2,199 Views
bh_lee
Contributor I

I want to know why error like the picture appears.

 

Also, what should I do to solve this error?

스크린샷 2024-11-21 093019.png스크린샷 2024-11-21 093019.png

스크린샷 2024-11-21 093906.png스크린샷 2024-11-21 093906.png

bh_lee_0-1732149557018.pngbh_lee_0-1732149557018.png

 

Tags (1)
0 Kudos
Reply
1 Reply

2,173 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @bh_lee,

Firstly, 

Could you please provide more details about how are you opening this project?

Is this an imported project from another version? If so, please check that the same S32DS version is used, since there are some differences in configuration that might affect build processes.

Did you create a new workspace and then open the project from another workspace? Or did you copy the project directory to the new workspace and then load existing project?

Did you use the import existing project wizard? Did you try a Clean Build command first?

By the screenshots, it seems that there are some undefined references to llibHYundaiApp IHWIA _SA_ASW_S32M276_V72. I suppose these are libraries, please check for includes in the properties of your project:

Julin_AragnM_2-1732295537672.pngJulin_AragnM_2-1732295537672.png

If possible, please share your project to test this on my side.

Best regards,
Julián

0 Kudos
Reply