S32M Knowledge Base

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32M Knowledge Base

讨论

排序依据:
Example Description This application demonstrates the usage FlexTimer Module in PWM Modulation Implementation mode. The application includes S32 Design Studio projects for both devices, that uses configurations for for the IP layer only (Clocks, Port_Ip_1 and Ftm_Pwm). For more details please refer to FlexTimer Module (FTM) Usage on S32M24x and S32K14x Series.   Installation steps Software installation      S32 Design Studio for S32 Platform v.3.5      RTD for S32K1 and S32M24x version 2.0.0 including patch P01 Hardware installation      Supported boards:           - S32M24xEVB-C064           - S32K144EVK      Connections to the scope in S32M24xEVB-C064/S32K144EVK:           - ftm0_ch0 -> PTD15 (J21-2/J2-2)           - ftm0_ch1  -> PTD16 (J21-1/J2-4)           - ftm0_ch2 -> PTD0  (J60-2/J2-6)           - ftm1_ch1   -> PTB3 (NA/J2-9) Not routable to an external pin in S32M244C_64LQFP      Debugger in S32M24xEVB-C064/S32K144EVK           - Use the On-board Debug Interface in J32/J7 Open SDA connector.   S32 Configurations Tool      Clocks Tool S32M244 and S32K144 features a complex clocking sourcing, distribution. To run a core of the S32M244/S32K144 as well as some MCU peripherals at maximum frequency 80 MHz in normal RUN mode, S32M244 is supplied externally by 16 MHz crystal (meanwhile S32K144 is supplied externally by 8 MHz crystal). This clock source supplies Phase-lock-loop (PLL), which circuit multiplies frequency by 20 in S32M244 (and by 40 in S32K144) and divides by 2 resulting 160 MHz frequency on output for both devices. PLL output is then divided by 2 to supply core and system (80 MHz), further divided by 2 and 4 to supply bus clock (40 MHz) and flash clock (20 MHz), respectively (See next Figure). Figure 1. S32M244 Clocks Configuration        Pins Tool In Pins Tool are selected the signals to use the FTM0 module as follows: Figure 2. S32M244 Pins Configuration        Peripherals Tool Below is the FTM0 configuration (the default configuration of the tabs that are not shown is used): Figure 3: FTM0 Hardware instance Figure 4: FTM0 Clock Configuration Figure 5: FTM0 Global Channel Configuration Figure 6: FTM0 PwmFtmCh Figure 7: FTM1 Clock Configuration Figure 8: FTM1 PwmFtmCh     Software implementation The application software functionality perform the following instructions (see Example 1): - Initialize Clock driver. - Initialize Port driver - FTM Modulation configuration - Initialize PWM drivers - Update periods for FTM0/1 - Update duty cycle to PWM signals Example 1. S32M244 FTM0/1 configured by S32 SDK int main(void) { /* Init clock () */ Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); /* Initialize all pins using the Port driver */ Port_Ci_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_BOARD_InitPins, g_pin_mux_InitConfigArr_BOARD_InitPins); /* FTM Modulation Implementation */ SIM_Type * simeBase = IP_SIM_BASE_PTRS; simeBase->FTMOPT1 = SIM_FTMOPT1_FTM0_OUTSEL(7); /* 0000_0111b channels 1, 2 and 3*/ /* Initialize PWM drivers */ Ftm_Pwm_Ip_Init(FTM_INSTANCE_1, &Ftm_Pwm_Ip_UserCfg0); Ftm_Pwm_Ip_Init(FTM_INSTANCE_0, &Ftm_Pwm_Ip_UserCfg0); /* Set new period for for Edge-Align Pwm */ Ftm_Pwm_Ip_UpdatePwmPeriod(FTM_INSTANCE_1, 0x500, TRUE); Ftm_Pwm_Ip_UpdatePwmPeriod(FTM_INSTANCE_0, 0x5000, TRUE); /* Setup new duty cycle to PWM signals */ Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_1, FTM1_CH_1, 0x250, 0x000, TRUE); Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_0, 0x4000, 0x000, TRUE); Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_1, 0x3000, 0x000, TRUE); Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_2, 0x2000, 0x000, TRUE); … }     On the oscilloscope Figure 9 shows ftm0_ch0 (D0), ftm0_ch1 (D1) and ftm0_ch2 (D2) signals of S32M244 on the oscilloscope. Such signals have the same period aligned in the edge, with different duty cycle and without PWM Modulation Implementation. Figure 9: Edge-align PWM (EPWM) mode without PWM Modulation Implementation (in S32M244) Figure 10 shows same signals from Figure 9, but now with PWM Modulation. Figure 10: PWM Modulation Implementation (in S32M244) Figure 11 shows ftm0_ch0 (D4), ftm0_ch1 (D5) and ftm0_ch2 (D6) signals of S32K144 on the oscilloscope. Such signals have the same period aligned in the edge, with different duty cycle and with PWM Modulation. Additionally this device allows to route externally the ftm1_ch1 (D7). Figure 11: PWM Modulation Implementation (in S32K144)  
查看全文
Example Description This application demonstrates the usage FlexTimer Module in Modified Combine mode for Phase Shift. The application includes S32 Design Studio projects for both devices, that uses configurations for for the IP layer only (Clocks, Port_Ip_1 and Ftm_Pwm). For more details please refer to FlexTimer Module (FTM) Usage on S32M24x and S32K14x Series.   Installation steps Software installation      S32 Design Studio for S32 Platform v.3.5      RTD for S32K1 and S32M24x version 2.0.0 including patch P01 Hardware installation      Supported boards:           - S32M24xEVB-C064           - S32K144EVK      Connections to the scope in S32M24xEVB-C064/S32K144EVK:           - ftm0_ch0 -> PTD15 (J21-2/J2-2)           - ftm0_ch1  -> PTD16 (J21-1/J2-4)           - ftm0_ch2 -> PTD0  (J60-2/J2-6)           - ftm0_ch3 -> PTD1   (J60-3/J6-2)      Debugger in S32M24xEVB-C064/S32K144EVK           - Use the On-board Debug Interface in J32/J7 Open SDA connector.   S32 Configurations Tool      Clocks Tool S32M244 and S32K144 features a complex clocking sourcing, distribution. To run a core of the S32M244/S32K144 as well as some MCU peripherals at maximum frequency 80 MHz in normal RUN mode, S32M244 is supplied externally by 16 MHz crystal (meanwhile S32K144 is supplied externally by 8 MHz crystal). This clock source supplies Phase-lock-loop (PLL), which circuit multiplies frequency by 20 in S32M244 (and by 40 in S32K144) and divides by 2 resulting 160 MHz frequency on output for both devices. PLL output is then divided by 2 to supply core and system (80 MHz), further divided by 2 and 4 to supply bus clock (40 MHz) and flash clock (20 MHz), respectively (See next Figure). Figure 1. S32M244 Clocks Configuration        Pins Tool In Pins Tool are selected the signals to use the FTM0 module as follows: Figure 2. S32M244 Pins Configuration        Peripherals Tool Below is the FTM0 configuration (the default configuration of the tabs that are not shown is used): Figure 3: FTM Hardware instance Figure 4: FTM Clock Configuration Figure 5: FTM Global Channel Configuration Figure 6: FTM PwmFtmCh (for Ch0 and Ch1) Figure 7: FTM PwmFtmCh (for Ch2 and Ch3)   Software implementation The application software functionality perform the following instructions (see Example 1): - Initialize Clock driver. - Initialize Port driver - Initialize PWM driver - Update period for FTM0 - Update duty cycle to PWM signals Example 1. S32M244 FTM0 configured by S32 SDK int main(void) { /* Init clock */ Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); /* Initialize all pins using the Port driver */ Port_Ci_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_BOARD_InitPins, g_pin_mux_InitConfigArr_BOARD_InitPins); /* Initialize PWM driver */ Ftm_Pwm_Ip_Init(FTM_INSTANCE_0, &Ftm_Pwm_Ip_UserCfg0); /* Set phase shift, update the period and set duty cycle */ Ftm_Pwm_Ip_SetPhaseShift(FTM_INSTANCE_0, FTM_CH_0, 0x5000, 0x0000, TRUE); Ftm_Pwm_Ip_SetPhaseShift(FTM_INSTANCE_0, FTM_CH_2, 0x5000, 0x1500, TRUE); /* Set phase shift and duty cycle value to PWM signals */ Ftm_Pwm_Ip_SetDutyPhaseShift(FTM_INSTANCE_0, FTM_CH_0, 0x2500, 0x0000, TRUE); Ftm_Pwm_Ip_SetDutyPhaseShift(FTM_INSTANCE_0, FTM_CH_2, 0x2500, 0x1500, TRUE); … }     On the oscilloscope Figure 8 shows that the ftm0_ch0 (D0), ftm0_ch1 (D1), ftm0_ch2 (D2) and ftm0_ch3 (D3) signals on the oscilloscope. Such signals have the same period and duty cycle aligned in the edge, but ftm0_ch2 is phase shifted with respect ftm0_ch0. Also, ftm0_ch1 is the complementary of ftm0_ch0 with inverted output. And ftm0_ch3 is the complementary of ftm0_ch2 with inverted output. Figure 8: Modified Combine mode for Phase Shift
查看全文
Example Description This application demonstrates the usage FlexTimer Module in Center-Aligned PWM (CPWM) mode. The application includes S32 Design Studio projects for both devices, that uses configurations for for the IP layer only (Clocks, Port_Ip_1 and Ftm_Pwm). For more details please refer to FlexTimer Module (FTM) Usage on S32M24x and S32K14x Series.   Installation steps Software installation      S32 Design Studio for S32 Platform v.3.5      RTD for S32K1 and S32M24x version 2.0.0 including patch P01 Hardware installation      Supported boards:           - S32M24xEVB-C064           - S32K144EVK      Connections to the scope in S32M24xEVB-C064/S32K144EVK:           - ftm0_ch0 -> PTD15 (J21-2/J2-2)           - ftm0_ch1  -> PTD16 (J21-1/J2-4)           - ftm0_ch2 -> PTD0  (J60-2/J2-6)           - ftm0_ch3 -> PTD1   (J60-3/J6-2)      Debugger in S32M24xEVB-C064/S32K144EVK           - Use the On-board Debug Interface in J32/J7 Open SDA connector.   S32 Configurations Tool      Clocks Tool S32M244 and S32K144 features a complex clocking sourcing, distribution. To run a core of the S32M244/S32K144 as well as some MCU peripherals at maximum frequency 80 MHz in normal RUN mode, S32M244 is supplied externally by 16 MHz crystal (meanwhile S32K144 is supplied externally by 8 MHz crystal). This clock source supplies Phase-lock-loop (PLL), which circuit multiplies frequency by 20 in S32M244 (and by 40 in S32K144) and divides by 2 resulting 160 MHz frequency on output for both devices. PLL output is then divided by 2 to supply core and system (80 MHz), further divided by 2 and 4 to supply bus clock (40 MHz) and flash clock (20 MHz), respectively (See next Figure). Figure 1. S32M244 Clocks Configuration        Pins Tool In Pins Tool are selected the signals to use the FTM0 module as follows: Figure 2. S32M244 Pins Configuration        Peripherals Tool Below is the FTM0 configuration (the default configuration of the tabs that are not shown is used): Figure 3: FTM Hardware instance Figure 4: FTM Clock Configuration Figure 5: FTM Global Channel Configuration Figure 6: FTM PwmFtmCh   Software implementation The application software functionality perform the following instructions (see Example 1): - Initialize Clock driver. - Initialize Port driver - Initialize PWM driver - Update period for FTM0 - Update duty cycle to PWM signals Example 1. S32M244 FTM0 configured by S32 SDK int main(void) { /* Init clock */ Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); /* Initialize all pins using the Port driver */ Port_Ci_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_BOARD_InitPins, g_pin_mux_InitConfigArr_BOARD_InitPins); /* Initialize PWM driver */ Ftm_Pwm_Ip_Init(FTM_INSTANCE_0, &Ftm_Pwm_Ip_UserCfg0); /* Set new period for PWM Signals*/ Ftm_Pwm_Ip_UpdatePwmPeriod(FTM_INSTANCE_0, 0x5000, TRUE); /* Setup new duty cycle to PWM signals */ Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_0, 0x4000, 0x000, TRUE); Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_1, 0x3000, 0x000, TRUE); Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_2, 0x2000, 0x000, TRUE); Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_3, 0x1000, 0x000, TRUE); … }   On the oscilloscope Figure 7 shows that the ftm0_ch0 (D0), ftm0_ch1 (D1), ftm0_ch2 (D2) and ftm0_ch3 (D3) signals on the oscilloscope. Such signals have the same period aligned in the center and with different duty cycle. Figure 7: Center-Aligned PWM (CPWM) mode
查看全文
Example Description This application demonstrates the usage FlexTimer Module in Edge-align PWM (EPWM) mode. The application includes S32 Design Studio projects for both devices, that uses configurations for for the IP layer only (Clocks, Port_Ip_1 and Ftm_Pwm). For more details please refer to FlexTimer Module (FTM) Usage on S32M24x and S32K14x Series.   Installation steps Software installation      S32 Design Studio for S32 Platform v.3.5      RTD for S32K1 and S32M24x version 2.0.0 including patch P01 Hardware installation      Supported boards:           - S32M24xEVB-C064           - S32K144EVK      Connections to the scope in S32M24xEVB-C064/S32K144EVK:           - ftm0_ch0 -> PTD15 (J21-2/J2-2)           - ftm0_ch1  -> PTD16 (J21-1/J2-4)           - ftm0_ch2 -> PTD0  (J60-2/J2-6)           - ftm0_ch3 -> PTD1   (J60-3/J6-2)      Debugger in S32M24xEVB-C064/S32K144EVK           - Use the On-board Debug Interface in J32/J7 Open SDA connector.   S32 Configurations Tool      Clocks Tool S32M244 and S32K144 features a complex clocking sourcing, distribution. To run a core of the S32M244/S32K144 as well as some MCU peripherals at maximum frequency 80 MHz in normal RUN mode, S32M244 is supplied externally by 16 MHz crystal (meanwhile S32K144 is supplied externally by 8 MHz crystal). This clock source supplies Phase-lock-loop (PLL), which circuit multiplies frequency by 20 in S32M244 (and by 40 in S32K144) and divides by 2 resulting 160 MHz frequency on output for both devices. PLL output is then divided by 2 to supply core and system (80 MHz), further divided by 2 and 4 to supply bus clock (40 MHz) and flash clock (20 MHz), respectively (See next Figure). Figure 1. S32M244 Clocks Configuration        Pins Tool In Pins Tool are selected the signals to use the FTM0 module as follows: Figure 2. S32M244 Pins Configuration        Peripherals Tool Below is the FTM0 configuration (the default configuration of the tabs that are not shown is used): Figure 3: FTM Hardware instance Figure 4: FTM Clock Configuration Figure 5: FTM Global Channel Configuration Figure 6: FTM PwmFtmCh   Software implementation The application software functionality perform the following instructions (see Example 1): - Initialize Clock driver. - Initialize Port driver - Initialize PWM driver - Update period for FTM0 - Update duty cycle to PWM signals Example 1. S32M244 FTM0 configured by S32 SDK int main(void) { /* Init clock */ Clock_Ip_Init(&Clock_Ip_aClockConfig[0]); /* Initialize all pins using the Port driver */ Port_Ci_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_BOARD_InitPins, g_pin_mux_InitConfigArr_BOARD_InitPins); /* Initialize PWM driver */ Ftm_Pwm_Ip_Init(FTM_INSTANCE_0, &Ftm_Pwm_Ip_UserCfg0); /* Set new period for PWM Signals*/ Ftm_Pwm_Ip_UpdatePwmPeriod(FTM_INSTANCE_0, 0x5000, TRUE); /* Setup new duty cycle to PWM signals */ Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_0, 0x4000, 0x000, TRUE); Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_1, 0x3000, 0x000, TRUE); Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_2, 0x2000, 0x000, TRUE); Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_3, 0x1000, 0x000, TRUE); … }     On the oscilloscope Figure 7 shows that the ftm0_ch0 (D0), ftm0_ch1 (D1), ftm0_ch2 (D2) and ftm0_ch3 (D3) signals on the oscilloscope. Such signals have the same period aligned in the edge and with different duty cycle. Figure 7: Edge-align PWM (EPWM) mode
查看全文