Example Description
This application demonstrates the usage FlexTimer Module in PWM Modulation Implementation mode. The application includes S32 Design Studio projects for both devices, that uses configurations for for the IP layer only (Clocks, Port_Ip_1 and Ftm_Pwm).
For more details please refer to FlexTimer Module (FTM) Usage on S32M24x and S32K14x Series.
Installation steps
Software installation S32 Design Studio for S32 Platform v.3.5 RTD for S32K1 and S32M24x version 2.0.0 including patch P01
Hardware installation Supported boards: - S32M24xEVB-C064 - S32K144EVK
Connections to the scope in S32M24xEVB-C064/S32K144EVK: - ftm0_ch0 -> PTD15 (J21-2/J2-2) - ftm0_ch1 -> PTD16 (J21-1/J2-4) - ftm0_ch2 -> PTD0 (J60-2/J2-6) - ftm1_ch1 -> PTB3 (NA/J2-9) Not routable to an external pin in S32M244C_64LQFP Debugger in S32M24xEVB-C064/S32K144EVK - Use the On-board Debug Interface in J32/J7 Open SDA connector.
S32 Configurations Tool
Clocks Tool
S32M244 and S32K144 features a complex clocking sourcing, distribution. To run a core of the S32M244/S32K144 as well as some MCU peripherals at maximum frequency 80 MHz in normal RUN mode, S32M244 is supplied externally by 16 MHz crystal (meanwhile S32K144 is supplied externally by 8 MHz crystal). This clock source supplies Phase-lock-loop (PLL), which circuit multiplies frequency by 20 in S32M244 (and by 40 in S32K144) and divides by 2 resulting 160 MHz frequency on output for both devices. PLL output is then divided by 2 to supply core and system (80 MHz), further divided by 2 and 4 to supply bus clock (40 MHz) and flash clock (20 MHz), respectively (See next Figure).
Figure 1. S32M244 Clocks Configuration
Pins Tool
In Pins Tool are selected the signals to use the FTM0 module as follows:
Figure 2. S32M244 Pins Configuration
Peripherals Tool
Below is the FTM0 configuration (the default configuration of the tabs that are not shown is used):
Figure 3: FTM0 Hardware instance
Figure 4: FTM0 Clock Configuration
Figure 5: FTM0 Global Channel Configuration
Figure 6: FTM0 PwmFtmCh
Figure 7: FTM1 Clock Configuration
Figure 8: FTM1 PwmFtmCh
Software implementation
The application software functionality perform the following instructions (see Example 1): - Initialize Clock driver. - Initialize Port driver - FTM Modulation configuration - Initialize PWM drivers - Update periods for FTM0/1 - Update duty cycle to PWM signals
Example 1. S32M244 FTM0/1 configured by S32 SDK
int main(void)
{
/* Init clock () */
Clock_Ip_Init(&Clock_Ip_aClockConfig[0]);
/* Initialize all pins using the Port driver */
Port_Ci_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_BOARD_InitPins, g_pin_mux_InitConfigArr_BOARD_InitPins);
/* FTM Modulation Implementation */
SIM_Type * simeBase = IP_SIM_BASE_PTRS;
simeBase->FTMOPT1 = SIM_FTMOPT1_FTM0_OUTSEL(7); /* 0000_0111b channels 1, 2 and 3*/
/* Initialize PWM drivers */
Ftm_Pwm_Ip_Init(FTM_INSTANCE_1, &Ftm_Pwm_Ip_UserCfg0);
Ftm_Pwm_Ip_Init(FTM_INSTANCE_0, &Ftm_Pwm_Ip_UserCfg0);
/* Set new period for for Edge-Align Pwm */
Ftm_Pwm_Ip_UpdatePwmPeriod(FTM_INSTANCE_1, 0x500, TRUE);
Ftm_Pwm_Ip_UpdatePwmPeriod(FTM_INSTANCE_0, 0x5000, TRUE);
/* Setup new duty cycle to PWM signals */
Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_1, FTM1_CH_1, 0x250, 0x000, TRUE);
Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_0, 0x4000, 0x000, TRUE);
Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_1, 0x3000, 0x000, TRUE);
Ftm_Pwm_Ip_UpdatePwmChannel(FTM_INSTANCE_0, FTM_CH_2, 0x2000, 0x000, TRUE);
…
}
On the oscilloscope
Figure 9 shows ftm0_ch0 (D0), ftm0_ch1 (D1) and ftm0_ch2 (D2) signals of S32M244 on the oscilloscope. Such signals have the same period aligned in the edge, with different duty cycle and without PWM Modulation Implementation.
Figure 9: Edge-align PWM (EPWM) mode without PWM Modulation Implementation (in S32M244)
Figure 10 shows same signals from Figure 9, but now with PWM Modulation.
Figure 10: PWM Modulation Implementation (in S32M244)
Figure 11 shows ftm0_ch0 (D4), ftm0_ch1 (D5) and ftm0_ch2 (D6) signals of S32K144 on the oscilloscope. Such signals have the same period aligned in the edge, with different duty cycle and with PWM Modulation. Additionally this device allows to route externally the ftm1_ch1 (D7).
Figure 11: PWM Modulation Implementation (in S32K144)
View full article