the differnence between this two command

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the differnence between this two command

2,112件の閲覧回数
814420552
Contributor III

Hello,

What's the difference between the following erase method?

pastedImage_1.png

I can't get the difference between this two comand,  wish your detail description!!

thanks

0 件の賞賛
返信
3 返答(返信)

2,007件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi kui wu,

"36.5.9.2 Flash commands" of S32K-RM.36.5.9.2 Flash commands.png

AN12130, Production Flash Programming Best Practices for S32K1xx MCUs - Application Note

AN12130.png

For more detail please read the "37.5.9.11 Erase All Blocks command" and "37.5.9.13 Erase All Blocks Unsecure command" of S32K-RM.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,007件の閲覧回数
814420552
Contributor III

hello, 

   pastedImage_1.png

      when execute this two command it will erase the P-Flash code, If it's erased, isn't it that the application won't run? Need to download the app again。

0 件の賞賛
返信

2,007件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi kui wu,

If it's erased, the MCU is blank no application run. The reset pin will toggle. Need to download the app again.

Best Regards,

Robin

0 件の賞賛
返信