the differnence between this two command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

the differnence between this two command

2,133 Views
814420552
Contributor III

Hello,

What's the difference between the following erase method?

pastedImage_1.png

I can't get the difference between this two comand,  wish your detail description!!

thanks

0 Kudos
Reply
3 Replies

2,028 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi kui wu,

"36.5.9.2 Flash commands" of S32K-RM.36.5.9.2 Flash commands.png

AN12130, Production Flash Programming Best Practices for S32K1xx MCUs - Application Note

AN12130.png

For more detail please read the "37.5.9.11 Erase All Blocks command" and "37.5.9.13 Erase All Blocks Unsecure command" of S32K-RM.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,028 Views
814420552
Contributor III

hello, 

   pastedImage_1.png

      when execute this two command it will erase the P-Flash code, If it's erased, isn't it that the application won't run? Need to download the app again。

0 Kudos
Reply

2,028 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi kui wu,

If it's erased, the MCU is blank no application run. The reset pin will toggle. Need to download the app again.

Best Regards,

Robin

0 Kudos
Reply