select clock for modules with PCC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

select clock for modules with PCC?

Jump to solution
3,032 Views
JeorgeB
Contributor III

Hi, 

 

I wanna to use LPSPI. assume there is a SOSC and Core CLK is 80MHz. bus clock is 40MHz. FIRC is 48MHz.

Can I use FIRC as input clock for LPSPI module ? (it is bigger than BUS CLK)

in page 566 for LPSPI, RM says : "Maximum frequency governed by BUS_CLK"

Thanks.

0 Kudos
Reply
1 Solution
2,992 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

AFigure 51-1. Block Diagram.pngFigure 51-1. Block Diagram.png

BFigure 10. LPSPI Example Block Diagram.pngFigure 10. LPSPI Example Block Diagram.png

CGC low power.pngCGC low power.png

C. The limitation is for Functional clock, not the clock after divider. Same limitation by using FIRC-48MHz (>40MHz BUS_CLK)

View solution in original post

3 Replies
3,021 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JeorgeB,

You can not use FIRC(48MHz) as input clock for LPSPI module as it is bigger than BUS_CLK(40MHz).

Maximum frequency governed by BUS_CLK.pngMaximum frequency governed by BUS_CLK.pngTable 27-9. Peripheral module clocking.pngTable 27-9. Peripheral module clocking.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

3,016 Views
JeorgeB
Contributor III
Hi Robin, A. what is BUS_CLK role in here? is it only for communication between Master and the module? B. If we gated off this clock [CGC], the module will be switched off (do not consume power)? or we should disable [PCS] clock? C. Assume we, use prescaler and SCK divider with register appropriate setting, and LPSPI SCK clock is 8MHz, is there same limitation by using FIRC-48MHZ? Thanks.
0 Kudos
Reply
2,993 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

AFigure 51-1. Block Diagram.pngFigure 51-1. Block Diagram.png

BFigure 10. LPSPI Example Block Diagram.pngFigure 10. LPSPI Example Block Diagram.png

CGC low power.pngCGC low power.png

C. The limitation is for Functional clock, not the clock after divider. Same limitation by using FIRC-48MHz (>40MHz BUS_CLK)