s32k312 example code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

s32k312 example code

6,249 次查看
coo
Contributor I

Hello.

I installed S32DS for S32 and Extensions.

I use s32ds 3.5 ver

When I choose "New --> S32DS Project form Example" menu, there is only for S32K358, 344.

Is there way to get S32K312 example project?

Thank you.

0 项奖励
回复
8 回复数

5,865 次查看
chenhua
Contributor II

跟着大佬们一起学习NXP

0 项奖励
回复

5,869 次查看
chenhua
Contributor II

看你们牛弹琴,我也学会了。

0 项奖励
回复

6,222 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport
 
Sorry for the inconvenience we bring you!
Seems that you are using S32K3 RTD 3.0.0 or higher.
It did not offer S32K312 examples when you choose "New --> S32DS Project form Example" menu.
You need to create S32K312 project by refer to S32K344.
or
Refer to S32K312 examples in S32K3 RTD 2.0.0 + S32DS v3.4.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

6,154 次查看
coo
Contributor I
I'm trying to download s32ds version 3.4 and use S32K3 RTD 2.0.0.
But there is only S32K3 RTD AUTOSAR 4.4 version 2.0.0 in s32ds extensions and updates, is this right?
0 项奖励
回复

6,151 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

I have installed S32K3 RTD 2.0.0 - 2.0.3 offline for S32DS v3.4. I am not sure whether S32K3 RTD 2.0.3 will be displayed in your S32DS Extensions and Updates. If not, please offline install S32K3 Real-Time Drivers Version 2.0.3.

0 项奖励
回复

5,893 次查看
John64
Contributor I
Hi Robin, 

 How to install the S32K312 example in S32DS v3.5?

In S32DS V3.5 Extensions and Updates the S32K3 RTD 3.0.0, and it included S32K344/358 example code not S32K312. 

5,870 次查看
chenhua
Contributor II

原来如此,怪不得呢。thanks 

0 项奖励
回复

5,884 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Yes. S32K3 RTD 3.0.0 and 4.0.0 did not offer S32K312 examples. You may need to create it by yourself. Fortunately FAE provides some examples here for RTD 3.0.0 S32K312: All Example S32K312 DS3.5 RTD-3.0.0